Hi Lisa,
yes I tried every setting in debug configurations. Without success.
I forget to mention that I use MSP430F148, Windows7 Prof. 64bit
Best regards,
Joachim
Other Parts Discussed in Thread: MSP430F148 , TPS3838 We are designing an energy meter using MSP430F148 . The problem now is how to detect there is a mains failure and to write the kwh data into the flash within a short span of time supplied by capacitors…
Other Parts Discussed in Thread: MSP430F148 Hello!
With a MSP430F148 I want to write in a 16-Bit DAC (Maxim Max5444).
With function "writeDACVAlue" , I can set the Chip-Select frame and the 8 clock cycles.
The oszi can confirm this.
The only…
Other Parts Discussed in Thread: MSP430F5524 , MSP430F148 I have an old design that used the MSP430F148. Its board includes a high density connector that includes the JTAG pins and is used for programming the device during manufacturing. I am making a new…
Yes, I agree. I opened up a recent MSP430 programming file that I had and it had the @4000 at the top as well. Which MSP430 is in your system? I believe we only have target programming files for MSP430F148 and MSP430F169.
Hi Brandon,
I tried to program a second target and 3rd targets too the problem is some times the board gets programmed or I get the error situation is like
say I got an eror message saying : security fuse blown in using IAR compiler and if the same p…
Other Parts Discussed in Thread: MSP430F148 Dear all,
I am working on msp430f148/149 series. In my board no interrupt is working but the same code is working on another board, i am sending the timer interrupt code.I have checked the hardware as well as…
Other Parts Discussed in Thread: MSP430F148msp430f148
Timer_B7
What is the difference between CCIxA and CCIxB?
The data sheets indicate connections can be made internally and exterally.
Externally: CCI0A, what external pin is it connected to? CCI0B…
Other Parts Discussed in Thread: MSP430F148 Hi,
Im using MSP430F148 and trying to interface AT45DB321C but little confused about the Modes 0 and mode 3 because the document SLAU049 dosent mention clearly about the modes ,
well I am thinking that U1TCTL…
Other Parts Discussed in Thread: MSP430F148 Hello!
I want to write a function, witch gets a 16bit value and write it out to an ADC.
The problem:
My debugger means, that U1TXBUF has the value 127 and any assignment
" U1TXBUF = firstEightBits" changes…