Hi Jessica,
2.) http://focus.ti.com/docs/prod/folders/print/msp430f167.html and http://focus.ti.com/docs/prod/folders/print/msp430f2274.html --> both devices have 32kBytes of Flash
1.) Why does it matter if the Flash is NAND or NOR in case of the embedded…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…
Hello:
I information and you give me a link error is not the same.
I try to do the following:
$ strace -o log opkg install dlp-sdk_2.0-r8.0_cortexa15hf-neon.ipk
1768.log.txt
View the log file found that there are several directories not create…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave
Hello Pavel,
EDIT: I didn't read past your first error. You already did this, and I didn't notice.
Pavel Hristov said:
We tried adding the following lines in io.h
#elif defined(__ MSP430F6726 __) #define __MSP430_6726__
For your first error, you…