Part Number: MSP430F2012 Other Parts Discussed in Thread: UNIFLASH Tool/software: Code Composer Studio Hi,
while trying to reduce the power consumption of my MSP430F2012 microcontroller, I tried to use the 32kHz ACLK clock as system clock (MCLK). After…
Part Number: MSP430F2012 Hi,
I intend to use a small MSP430F2012 to read out a DC potmeter value and transmit that over a SPI in slave mode.
Since I have one SPI master and a total of four SPI slaves in my system I want to use the STE pin to disable the…
Part Number: MSP430F2012 Tool/software: Code Composer Studio Hi,
I wanted to fix a bug in a MSP430F2012 project I made some years ago on the IAR tools.
In the mean time I switched to CCS7 but when I import the project (only one C-file and one header file…
Part Number: MSP430F2012 Good afternoon....
Does the MSP430F2012 have ESD protection on the DIO pins?....I was hoping to use a 10k series resistor between a pin and an 8V switch to detect when the switch was thrown...The MSP will be powered off of 3.3V…
Part Number: MSP430F2012 Other Parts Discussed in Thread: MSP430F2013 , CCSTUDIO
Tool/software: Code Composer Studio
Using previous versions of CCS 7, one could select various Erase Options when using a MSP430F2012 device.
Using CCS V8.3 there are no…
Part Number: MSP430F2012 Other Parts Discussed in Thread: CC1150 , Hi to all,
Had to add temperature reading to an earlier project by reading a voltage from half bridge formed by fixed resistor and NTC. It is battery powered device so I wanted to use P1…
Hello Ali,
Thanks for posting your question to E2E. Sigma Delta and SAR ADCs are used for different reasons. Generally, Sigma Delta ADCs offer high resolution but slower sampling rates compared to SAR ADCs. Take a look at the following (dated but still…
Part Number: MSP430F2012 Customer use SBW mode to Read/Write MSP430F2012 flash from host. The project is in mass production for about 10 years without problem. But recently, they got 100pcs boards failed in SBW Read/Write among 500 pcs board. SBWTCK and…
Other Parts Discussed in Thread: MSP430F2012 Hi all !
I have a problem programming MSP430F2012 (not all but some uC on the same kind of board) with MSP-FET430UIF via 2-wire JTAG mode, using MSP430Flasher.
I tried both old and new firmware of the tool but…
Other Parts Discussed in Thread: MSP430F2012 , MSP-FET , MSP-TS430PW28A , MSP430G2553 Hi everyone, sorry for my English.
I have the MSP430F2012 and programmer MSP-FET. I connected it according to the scheme
I use CCSv6 and FETPro430-Lite. I tried to blow fuse…