Other Parts Discussed in Thread: MSP430F2012 Hi all !
I have some issues programming MSP430F2012 uC using 2-wire JTAG by MSP-FET430UIF tool. Programming (on automatic test bench, via spring test probes) on some uC (not all, because many program without…
we’re planning to use the internal clock of the MSP430F2012IRSAT micro. Per Figure 5-1 on page 274 of the User’s Guide (SLAU144J), we thought about using the MCLK output for this. It appears that we should be able to set the appropriate registers to create…
Other Parts Discussed in Thread: MSP430F2012 , TMP112 I'M STARTING A PROJECT USING MSP430F2012 AND TMP112 AS SLAVE. DOES SOMEBODY HAS A CODE EXAMPLE HOW TO INITIALIZE THE MSP430F2012 TO SETUP THE COMMUNICATION IN I2C?
Dennis:
Here is my code that works fine on the F2012 but hangs on the G2332. Also note that the IAR Workbench debugger shows the memory at 0x1000 to be alternating 0xFF and 0x3F through ox10FF after the
dummy write.
Thanks
Al
void write_SegD (void) { …
Other Parts Discussed in Thread: MSP430F2012 I am in need of a parameter file for programing Texas Instruments MSP430F2012 chips with my Renesas PG-FP5 any help would be appreciated
Other Parts Discussed in Thread: MSP430F2012 hi,
the spec list in TI website shows MSP430F2012 has UART BSL, but checking its datasheet can not found which pins are BSL_TX and BSL_RX, that makes me confused is it exist ROM based BSL in MSP430F2012?
Hello,
A customer of mine is using the MSP430F2102 (RSA package). After power-up, pin 1 (ADC) outpus current and it is not programmed to output current.
On pin 1 there is a 470 ohm resistor to 24V and a 47K resistor to gnd. This results in 2.18V on the…
When P1IFG is set depends not only on P1IN but also on P1IES. Also, changing P1IES may set P1IFG. The interrupt edge detection logic is quite simple. Any configuration or state change may cause an ‘edge’ being detected.
Other Parts Discussed in Thread: ENERGYTRACE , MSP-FET I just started using a MSP-FET and started to use it to profile the power consumption in my design. In LPM3, it shows ~ 30uA. I was surprised (since the design was previously benched with a multimeter…
Other Parts Discussed in Thread: MSP430F2012 While using MSP430F2012 in my projekt, I have a current consumption problme in LPM3 mode.
After initialization of the CLKs and ports, I use the ADC10 to measure the power supply of the MSP and use this command…