Part Number: MSP430F2013 Good morning,
I have a problem in configuring the internal reference Vref = 1.2 V of the ADC SD16_A as an output in the microcontroller MSP430F2013. Indeed, following the datasheet, I set the bits SD16VMIDON = 1 and SD16REFON…
Part Number: MSP430F2013 Hi Team,
Customer want to know how MSP430F2013 DC0 clock configuration translate into register values. Customer details below.
"
In the C programming examples i am using the internal clock DC0 is configured in a way I do not…
Part Number: MSP430F2013 Hello expert,
our customer asked a question regarind the QFN pad for MSP430F2013,
They know TI recommedens to connect this pin to GND, but if this pin becomes open,
what kind of the risk they need to consider? Also, does TI have…
Part Number: MSP430F2013 Other Parts Discussed in Thread: LF398-N Well,
I put the MSP430F2013 SD converter in internal VDD or temp sensor conversion mode loop and pulse a pin at the end of conversion
and I note that at the lowest oversampling rate of…
Part Number: MSP430F2013 When running code on an MSP430F2013 for a sensing application we have firmware that runs at 8MHz using the internal oscillator and calibrated register. However, the datasheet indicates the maximum clock speed for the SD16 module…
Part Number: MSP430F2013 Tool/software: Code Composer Studio Dear colleagues, is there an example code which shows how to use the I2C-Interface (as master) without using interrupt? Would be nice. Franz Peter
Part Number: MSP430F2013 Other Parts Discussed in Thread: UNIFLASH , , MSP-FET , MSP430F2012 Tool/software: Code Composer Studio I have three custom MSP430F2013 boards, all the same. Two can be programmed with CCS V10 / MSP-FET/SBW without issue, but the…
Part Number: MSP430F2013 Other Parts Discussed in Thread: MSP-EXP430G2ET Hello,
I am trying to use the SD16 on the F2013 to measure Vcc internally on channel A5, but I keep getting measurements around 2.7 V to 2.8 V when I am powering with 3.3 V. I am…
Part Number: MSP430F2619 Other Parts Discussed in Thread: MSP430F2013 Hi Team,
We have planned to use below parts in my design. Could you please provide these details INL, Offset Drift and Gain Error drift.
Kindly please find below part numbers.
1)MSP…