Hi Will, Thanks for the reply. I made a SBW connection to the MSP430F2101. The chip does not support SBW, only 4 wire JTAG.
So yes I have made a mistake. Sorry for the inconvenience.
Kind regards, Cor
Other Parts Discussed in Thread: MSP430G2101 , MSP430F2101 I'm bringing up a board which uses the MSP430G2101 microcontroller, and I'm using IAR Kickstart. However, I don't see the device listed; the closest I see is the MSP430F2101. Is this…
Other Parts Discussed in Thread: MSP430F2101 Hi, i am using the MSP430F2101 i would like to enable timer with external event, so someone tell me to use interrupt to activate the timer, how i do this, the external event is a pin set to 1, HELP please i don…
Other Parts Discussed in Thread: MSP430F2101 I'm using CCS 4.2.4.00033 with Grace 1.00.01.83 under a Win7 32 Bit environment. Because this is my first project with Grace, I wanted to test it a Grace example project (blinking LED with TimerA). So I simply…
Other Parts Discussed in Thread: MSP430F2101 , MSP430G2452 , MSP430G2101 Hi:
I´m using a Gang programmer to program MSP430Fxx with firmwaqre version 1.53, We need to program MSP430G2452 and MSP430G2101, I´ve made a upgrade of firmware to 1.54 firmware,…
Other Parts Discussed in Thread: MSP-TS430PW28 , MSP430F2101 I just tested the supplied Grace examples. "Blink LED from the CPU" is working as intended, but "Blink LED from Timer_A interrupt and CPU" isn't working at all. My LED always stays dark. But because…
Other Parts Discussed in Thread: MSP430F5528 , MSP430F2101 Hi,
I want to program an MSP430F2101 from a MSP430F5528 via the BSL using TEST/RESET. It would seem this should be quite possible using the on-chip UART in the 5528. I've been reading "MSP430 programming…
Your
MSP430F2101
will do both PWM channels simultaneously while enforcing dead time. You won't need to synchronize 2 MSP430 devices. Just 1 is enough for the job.
Jeff
L here. I looked into the file, the .c, and changed the #include "msp430f2101.h" to #include "msp430g22311.h". Duh, keep the basics.
I apologize to anyone who may have answered. Please no replies to this. And I read up on this C2000…
i like to synchronise two PWM signal between two MCU http://focus.ti.com/lit/ds/symlink/msp430f2101.pdf , this mcu are located in two different place and supplied with two battery cell, so i used to output the clock of mcu1 and this will be the clock for…