Part Number: MSP430F2121 Hi Team,
Issue: the monolithic information is lost or erased.
The crystal output frequency is 19.999992 MHz at the time of power-up, which meets the 20 MHz ± 10 Hz requirement. The crystal output frequency is 20.000092 MHz after…
Part Number: MSP430F2121 Other Parts Discussed in Thread: MSP430FR5870 , MSP-FET , MSP-FLASHER , MSP-GANG Dear Team,
We have used MSP430F2121 and MSP430FR5870 MCUs in our Products. Currently MSP-FET is being used to Program the MCUs during development.
…
Part Number: MSP430F2121 Hi experts,
Please let me confirm the marking information on the back of the device package.
In the following two devices, the direction of the marking is different by 180°.
Model number: MSP430F2121IPW, TSSOP(PW) | 20 The…
Part Number: MSP430F2121 Other Parts Discussed in Thread: MSP430F1121 , , MSP430F1121A Hi
I use for a long time the MSP430F1121 but alas this one is obsolete. my programming platform is a simple BSLDEMO UART V24 interface. Can I consider directly implementing…
Mainly because I want to use the Spy-Bi-Wire interface. But when I simply swapped the chips, it did program over traditional JTAG, but the application didn't work.
Did I miss something in the pinouts or config registers?
Other Parts Discussed in Thread: MSP-TS430PW28A , MSP-TS430PW28 hi team, please, i need your help, regard the MSP-FET430U28A, it is an KIT Emulator and programmer . My question is: this kit is right for to develop on platform MSP430F2121PW. best regards Pi…
Other Parts Discussed in Thread: MSP430F2121 Hello everyone,
i'm trying to get a software uart solution with the MSP430F2121 working.
Ive started with the code example from TI (msp430x21x1_ta_uart19200_1MHz.c), but in my application I dont have a 32…
i am reviewing code to used on an MSP430F212RGE device and noticed the following port initialization:
mov.b BIT3, $P2DIR
mov.b (BIT7+BIT6+BIT3), &P2SEL
...
mov.b BIT3, &CAPD
1. Is there any problem having P2DIR.bit3 = 0, P2SEL.bit3 = 1, and CAPD…
Other Parts Discussed in Thread: MSP430F2121 Hi Folks,
I am contemplating a move to the 'value line' for a product which uses the MSP430F2121. It uses Timer_A3 to generate pulses from the 'TA' pin. But the '430G23x2 family has completely mixed up the…
Other Parts Discussed in Thread: MSP430F2121 hi all am having msp430f2121 20 pin controller.. and am having msp-exp430g2 kit and eZ430-F2013 kit.. i need to know whether it s possible to program the msp430f2121 controller with the help of above two kits…