Part Number: MSP430F2122 Other Parts Discussed in Thread: MSP430F1232 , MSP430F2234 1) I have couple of older UIF's. (MSP-FET430UIF V 1.4A)
2) I have updated the firmware.
3) I can use them to program and debug successfully (with breakpoints) the MSP430F2234…
Part Number: MSP430F2122 Other Parts Discussed in Thread: MSP430WARE
Tool/software: TI C/C++ Compiler
Hi everyone,
Why is there a error shown as the following figure when I import an old project?
I have built a project in the past and it can work normally…
Part Number: MSP430F2122 Tool/software: Code Composer Studio Hello Everyone,
I use CCS6 to edit my old projects which was created by CCS4 late in the days.
But I have some troubles while I doing "Debug".
I press DEBUG, and there is a message…
Hi Caleb Overbay,
I have checked this.
It is MSP430F2122, and the same project can debug with other MSP430F2122 chip without any error.
What kind of problem can cause this trouble?
Does the chip have a bad paste on the pad or PCB?
This is a new project…
Hello Peter,
Thanks for sharing the customer's feedback and for digging. While the MSP-TS430RHB32A target socket board will accept 32-pin QFNs, the pin connections won't match up with the QFN package of the MSP430F2122 device, so they won't be able to…
Part Number: MSP430F2122 Other Parts Discussed in Thread: MSP-EXP430F5529LP , MSP-FET Hi,
I connect SBW signals of eZ-FET Lite (MSP-EXP430F5529LP) to MSP430F2122 which install to my board. The ccs flash failed to F2122, it will show "Error connecting to…
Other Parts Discussed in Thread: MSP430F2122 Hello everyone!
Is the first time when i work with the MSP430 MCU's and i don't know much about them.
I'm trying to make a led blink ( on PORT 1.6 of MSP430F2122 ) with timers. It works fine with…
Other Parts Discussed in Thread: MSP430F2122 Hi all,
I am trying to run an MSP430F2122 with an 12 MHz crystal on XT1, but without success. The oscillation doesn't start.
Here is my code, it's like in the example:
WDTCTL = WDTPW + WDTHOLD; // Stop…
Hello,
I think I fried the MSP chip on the eval board, and I'd like to replace the chip. I'd like to be able to program it with the code it had before, but I can't find even a binary. Does anyone know where I can get this?
Thank-you,
-I. Jantz…