Hello,
I think I fried the MSP chip on the eval board, and I'd like to replace the chip. I'd like to be able to program it with the code it had before, but I can't find even a binary. Does anyone know where I can get this?
Thank-you,
-I. Jantz…
Other Parts Discussed in Thread: MSP430F2122 Hello,
I have a problem with Timer1 on MSP430F2122 - it doesn't start. I have no idea where is the bug. I wrote simple example to check it, but still nothing. Code below. I am using IAR 4.11.
#include "msp430x21x2…
On interrupt, some things happen implicitely. The LPM bits and the GIE bit are cleared. So teh CPU will wake upt (just to execute the interrupt) and no other interrupts can interfere.
I don't know why this should affect P2.6/P2.7. Yes, OSCOFF is cleared…
Other Parts Discussed in Thread: MSP430F2112 , MSP430F2122 Dear All,
I am currently porting on of our older projects from Code composer 3.5 to 5.1.
(99.9% sure I am running the latest software / compiler as the update program has nothing the install)
Every…
Other Parts Discussed in Thread: MSP430F2122 Hi,
i'm new with this micro (msp430f2122) and i'd like to realize an adc conversion of two signals that i monitor on pins p2.0 and p2.1 trough a resistor divider.
The signals can vary from 0 to 10V…
Other Parts Discussed in Thread: MSP430F2122 Dear Helpdesk,
I am using MSP430F2122, there are only PORT1_VECTOR and PORT2_VECTOR macro for pin interrupt.
After the hardware design is fix I then realised that PORT3_VECTOR cannot be configured as interrupted…
Other Parts Discussed in Thread: MSP430F2122 Hi to everybody,
I am going to use 3 of the 8 channels that MSP430F2122 ADC has, but would I be able to use the other 5 channels for other purposes like digital inputs/outputs, PWM, at the same time?
I mean…
Other Parts Discussed in Thread: MSP430F2122 , BQ76925 , BQ76925EVM Hi all,
I am using the msp430 and BQ76925 to monitor individual cell voltages, pack current and temperature. I already attained the BQ76925EVM. The host MCU of EVM is the MSP430F2122.…
Other Parts Discussed in Thread: MSP430F2122 Hi,
I'm trying to program a MSP430F2122 with a MSP-FETU430IF JTAG flasher under a CCS4.2 environment and am running into a wall.
The exact type of MSP I'm using is very memory constrained (512 Bytes RAM…
Other Parts Discussed in Thread: MSP430F2122 , MSP430F2112 I have designed a ZigBee wireless module for industrial applications using the /MSP430F2122 and Digi wireless module. The MSP430F2122 chip is programmed through a 4 pin SpyWire cable attached to…