Other Parts Discussed in Thread: MSP430F2232 HI
i used launchpad to build a BSL programmer for msp430f2232.
I downloaded firmware from ti slau319 , and used BSLDEMO2.exe to
program my board with msp430f2232.
The problem :
after launchpad-bsl download…
Hi Community member,
Please let me confirm the following question.
[Question]
Would you please provide the data of wake-up time from each LPMs?
LPM0:
LPM1:
LPM2:
LPM3: 2us
LPM4: TBD. Depends on the crystal stable time.
Note: I could find the LPM3…
Other Parts Discussed in Thread: MSP430F2232 Hi,
We are currently facing issue in SPI chip select of TI MSP430F2232 USCI_A0 module.
Here we have initialized USCI_A0 module in slave SPI 4 wire mode by setting UCMODEx = 0x02 in USCI_A0 Control Register…
Other Parts Discussed in Thread: MSP430F2232
Dear
Sir,
We
are one of the leading manufacturers of Electronic weighing scales.
We
are under continues process of RND for our weighing needs.
Presently
we are developing new model with high accuracy…
Other Parts Discussed in Thread: MSP430F2232 I got a problem in ADC function of MSP430F2232.
CONDITION :
(1). use internal reference voltage for ADC of MSP430F2232. (ref = 2.5V)
(2). use Pin 26 (A7) for external voltage moniting.
(3). external voltage…
Hi,
What voltages should I expect on Xin and Xout (LFXT1) using a 32768Hz crystal? I have measured 400mV offset 200mV peek-peek on Xout and same but 0V as offset on Xin. Is this ok? Other MSP430 members I have used has much higher offset voltages. When…
Other Parts Discussed in Thread: MSP430F2232 , MSP430F2013 Hi,
I am trying to run my msp430f2232(mclk) at the frequency 16MHz, however it continuously gets reset, and goes to NMI_ISR routine(the value of IFG1 is 0x06, power on interrupt + oscillator fault…
Other Parts Discussed in Thread: MSP430F2232 Hi, i have been working on a datalogging project ( MSP430F2232 + Temperature sensor + I2C memory) and i have a really big problem with ther timer B.
I'm using the overflow option in the interruption on LP3…
Other Parts Discussed in Thread: MSP430F2232 Hi,
I am writing an application for the MSP430F2232. I am considering using the calibrated DCO frequencies but want to validate them before use. The MSP430x2xx user guide (slau144e) includes a routine for checking…