Other Parts Discussed in Thread: MSP430F235 Hi
In one of our applications using the MSP430F235, the supply voltage somtimes drops with a rate of about 100 mV/s towards 0 V. In that case the Brownout Reset is not triggered, which causes some problems.…
Other Parts Discussed in Thread: MSP430F235 , MSP430F5438 Hello team -
I am moving this discussion to the MSP430 forums for my customer since it looks like more of a MSP430 issue at this point than a Linux problem.
Please reference this thread in the…
Chapter 9 of the User's Guide says:
The SVS is implemented in selected MSP430x2xx devices.
None of them is in the G2xx "value line": MSP430AFE221, MSP430AFE231, MSP430AFE233, MSP430AFE253, MSP430F233, MSP430F235, MSP430F2416, MSP430F2417, MSP430F2418…
Other Parts Discussed in Thread: MSP430F235 The new version of CCS (6.1.2.00015) does not successfully link a program which works fine with CCS 5.5.0. The part we use is the MSP430F235, which is the correct part listed in the linker cmd file: -l msp430f235…
Hi Mano,
I am trying to keep BSL password for MSP430F235 fixed and trying to use the above method. Could you please help me sending sample of modified linker file that does this.
Thanks heaps.
Padma
Thank you Caleb,
Looking at the power line with a scope during I2C communication only shows very small perturbations (<50mV) in the supply voltage, as would normally be expected. I have also left a scope on an active device for 24 hours to look for more…
Other Parts Discussed in Thread: MSP430F235 , MSP430FR5969 Hi,
I try to implement MSP430FR5969 timer and watchdog timer code in proteus 8 professional tool. But it doesn't work. It shows an error. Even i try to implement MSP430F235 codes but that…
Other Parts Discussed in Thread: MSP430F235 Hi all,
I have a problem with detecting of XT2-oscillator fault in the MSP430F235. If I try to use interrupt NMI_VECTOR (I use IAR C-compiler) => interrupt go on immediately! WHY??? My code is below:
__bic_SR_register…
Other Parts Discussed in Thread: MSP430F235 Hi,
I´m using the MSP430F235 in my design. My question, is the /RST Pin nessesary for the jtag or optional?
If optional i will pullup the pin to 3,3V with a 47kOhm resistor.
Thanks in advance!
Gautham,
PWM is needed only if I want to control the speed of motor. For my application, that is not necessary. In that case, is it okay to drive the PWM pin high(in other words 100% duty cycle) from a GPIO of a MSP430F235?
I only want to turn on/off…