Part Number: MSP430F247 Hi: I would like to program the MSP430F247 using a serial UART inferface. I have connected the programmer to the MSP430F247 as follows: Programmer MSP430F247 UART_TXD RXD (P2.2)(Pin 22) UART_RXD TXD (P1.1)(Pin 13) …
Part Number: MSP430F247 Please help me with this I am not able to proceed.
// Clock Setup // -- Setup Clock to 16 MHz
__bic_SR_register(OSCOFF); // enable LFXT1 oscillator
BCSCTL1 |= XT2OFF + XTS; // LFXT1CLK is High Frequency BCSCTL3 |= LFXT1S0 + LFXT1S1;…
Part Number: MSP430F247 Tool/software: Code Composer Studio Is there a way to use the timer B (MSP430F247) like a "programmable frequencies generator" (I need 3 different and programmable frequency signals on TB0, TB1 and TB3) without using the interrupt…
Part Number: MSP430F247 Hi
Product #: MSP430F247TPMR
The following waveform was captured at device power on.
When powering on the device, crystal oscillator ( Green waveform ) behave like in the red box (in the waveform below) after releasing the CPU reset…
Part Number: MSP430F247 Hi team,
Questions from my customer
One of the significant error sources in their design is the ADC Integral Linearity Error of +/-1.7 LSBs maximum. Could you provide more details regarding the +/-1.7 LSB specification:
The +…
Part Number: MSP430F247 Hi
What is the allowable output current in each case of output Low and High for each port?
(I would like to know information , such as, x mA per terminal when output is low, and x mA when output is high.)
Thanks and Best regards…
Part Number: MSP430F247 Hi
Just after the device power-up, what is the state of each pins until the internal pull-up/down becomes valid?
Thanks and Best regards,
HaTa.
Part Number: MSP430F247
To Whom It May Concern:
There was a problem with the product purchased at the TI store. I contacted the Customer Support Center and was asked to submit a request here. Order number : T00599956 The orientation of the product in…
Part Number: MSP430F247 Other Parts Discussed in Thread: MSP-FET , MSP430G2553 I have programmed the MSP430F247 with MSP-FET programmer with the atprogram.exe with parameter -f (this is fuse activated).
We now want to change the program but it says is…