Part Number: MSP430F2617 We have found a MSP430F2617 microcontroller with faulty bits in the RAM memory. After a lot of debugging, it appears that the faulty bits are influenced by the values of their neighboring bits (as described below).
The batch is…
Part Number: MSP430F2617 Other Parts Discussed in Thread: DRV8846 Hello,
I'm new in the field and I need some advices. I bought a DRV8846 Evaluation Module to control a stepper motor. My aim is to modify the stepping time of the motor, so letting it always…
Part Number: MSP430F2617 Tool/software: Code Composer Studio I recently got the FET430UIF2 SBW programmer to program the MSP430F2617 controller.
However MSP430F2617 only supports 4 wire JTAG and not the 2 wire SBW offered on the UIF2.
I'm in need of a immediate…
Part Number: MSP430F2617 Hi,
I have a customer working on downloading firmware into MSP430F2617. According to the TI doc SLAU319N they need to use 2 pins: RST/NMI and TEST to be able to enter to BSL (internal Boot Streep Loader). But there is no TEST…
Part Number: DRV8428EVM Other Parts Discussed in Thread: MSP430F2617 , , DRV8428 Hi;
Recently I was worked out DRV8428EVM .I have a doubt about regarding Software configuration due to we should interface the drv8428 with LPC1768 Microcontroller. In that…
Part Number: MSP430F2617 Hello,
This has reference to the MSP430F2617 errata sheet. It mentions the following problems XOSC5, XOSC6 and XOSC8.
As an example, XOSC5 is stated below:
"Function LF crystal failures may not be properly detected by the oscillator…
BTW, I down loaded the firmware (slvc831.zip) for the DRV8251AEVM eval board from the TI website. I unzipped to a personal folder and have attached a screenshot of the folder contents which show both a MSP430F2617.cmd file and a MSP430FR2100.cmd file…
Part Number: MSP430F2617 I have the following setup:
ADC12 is used with internal 2.5V reference. The input is channel 0 connected to an external pin that can go as high as 5V.
Given that the voltage limit on the external pin as AVCC + 0.3V, this is certainly…
We are using MSP430F2617T microcontroller in one of our products. Multiple units from the latest production batch (rev H chips) seem to exhibit a problem where temperature sensor reads incorrect temperature. For example factory calibration data as read…
Other Parts Discussed in Thread: MSP430F2617 , MSP430WARE I'm still having trouble getting my MSP430F2617 to work with an external 16 MHz oscillator. Thanks for the earlier comments. The MSP430F261x and 241x data sheet(SLAS541K) indicate the ability…