Part Number: MSP430F2618-EP Hi,
We are using MSP430F2618TGQWTEP which is part of the MSP430F2618-EP family. But according to web site and PDN (20191218000.3), this part will discontinue.
What is the difference between MSP430F2618-EP and MSP430F2618?
In web…
Part Number: MSP430F2618-EP Dears:
After welding and baking at 120 C for 2 hours, can MSP430F2618-EP bear it?
Will Flash flip and cause program errors or other problems?
Part Number: MSP430F2618-EP When using the MSP430F2618 as an SPI slave and needing to also use either another SPI or i2c as master, which protocol for master port would be most efficient? For example, if you were recieving communication from an external…
Part Number: MSP430F2618-EP Hi,
I know the information for reading out the chip revision (along with other information such as Year and Month Date Code, LOT Trace Code, and Assembly Site Code) from the package marking can be found in the device specific…
Part Number: MSP430F2618-EP Dear Team,
Can you please advise if we have any information on the flash data retention of the MSP430F2618TGQWTEP across temperatures ?
Customer is interested how this number is changed in high/low temperatures.
Best regards…
Part Number: MSP430F2618-EP I'm having an issue with the MSP430F2618-EP (REV H) during product operational high-temperature burn-in (+70C). The product appears to be non-responsive after a power cycle during the high temperature cycle, however the low…
Part Number: MSP430F2618-EP Hi, hope someone could help me.
I try to get my code from MSP430F169 to MSP430F2618.
The UART logic has changed for this microcontroller and I tried it with below code.
I have not found a TX-Enable in the 2618, like in the…
Rami,
I suspect the markings would be equivalent to ZQW. These should be the same package, but slightly different part numbers as I believe you have the EoL MSP430F2618-EP, which the only real difference is extended temperature range.
TI Team,
Is there an evaluation board that I can use for the MSP430F2618-EP? If not, perhaps there is a board that I can use and then drop in a version of the MSP430F2618-EP? Any recommendations are greatly appreciated?
My application requires rugged version…
Other Parts Discussed in Thread: MSP430F2618 Hello Fellows,
Could you explain me what is the temperature range of the MSP430F2618-EP. As soon as this MCU is part of the enhanced products microcontroller I expect that temperature range is -55...+125C …