Part Number: MSP430F2619S-HT Hello,
I am looking for the GPIOs state during reset for MSP430F2619S-HT. I found in the forum that IOs are configured as inputs but I need to know if there is a pull up or pull down or nothing while the component is kept…
Part Number: MSP430F2619S-HT Hi Everyone,
I'm trying to find a way to add a simple CRC16 to my program. The linker doesn't seem to offer the right options (it only provides CRC tables that add too much junk into the output file - every byte counts…
Part Number: MSP430F2619S-HT This is more of a feature request than a question. My apologies if this is not the correct location for such a request.
Here is what I would like to do.
We have applications that use LVDTs/RVDTs. To excite the primary of…
Part Number: MSP430F2619S-HT Other Parts Discussed in Thread: MSP-TS430PM64 , MSP-FET Hello,
Is there an evaluation board for MSP430F2619SPM?
TI or other?
Thanks,
Emmett
Part Number: MSP430F2619S-HT Hello-
We have dozens of fielded units utilizing the above microcontroller with 1000's of hours logged with no issues. Recently, a unit was sent back as unresponsive. After debugging power rails and all other support circuitry…
Part Number: MSP430F2619S-HT Dear Sir
I feed an external 8MHZ clock signal to the XT2IN pin for the MSP430F2619S-HT with below configuration:
BCSCTL3 = XT2S_3; // select external clock singal: 8MHZ
BCSCTL1 &= ~XT2OFF; //XT2OFF = 0
BCSCTL2 = DIVM_0…
Part Number: MSP430F2619S-HT Does this micro really support the Spy-Bi-wire debug interface ? The documentation seems to suggest that it does, but there is no indication that it does from the pin names. That is, none are defined as SBWTDIO and SBWTCK…
Part Number: MSP430F2619S-HT We are having some issues with the msp430f2619s-ht writing to the internal flash at high temperature and would appreciate any feedback/suggestion on what the problem might be and how to mitigate it ?
we have been investigating…
Part Number: MSP430F2619S-HT Hi, My customer reported strange behavior on their custom board. When below simple program runs, pulses are generated on P6.4. #include <msp430.h>
int main(void)
{
WDTCTL = WDTPW + WDTHOLD;// Stop watchdog timer
…