Part Number: MSP430F2619S-HT Hi, I would like to know what is the power consumption for running this IC at 32.768 kHz with 3.3V? Datasheet stated that this device will consume: Active Mode: 365 μA at 1 MHz, 2.2 V.
Part Number: MSP430F2619S-HT Hi Team,
The absolute maximum operating voltage of MSP430F2619SPM is 4.1V as stated in the datasheet and the recommended operating condition is 3.6V (max). Our customer would like to know if there are any concerns or significant…
Part Number: MSP430F2619S-HT Other Parts Discussed in Thread: MSP430WARE Hi,
I read application note SLAA336A with great interest. Calibrating the DCO at startup would be helpful in our application, since the DCO can vary quite a bit with temperature…
Part Number: MSP430F2619S-HT Hi Team,
My Customer is attempting to communicate with the MSP430F2619SPM device during testing at cold temperatures (around -40C), and are occasionally seeing a loss of the capability to communicate with this component during…
Part Number: MSP430F2619S-HT Other Parts Discussed in Thread: MSPDS , REP430F , MSP-FET , MSP430F5528 , MSP-EXP430FR5739 , ENERGYTRACE , UNIFLASH
Has anyone been able to build the eZ-FET firmware from the source files provided here: http://www.ti.com/tool/M…
Part Number: MSP430F2619S-HT Other Parts Discussed in Thread: MSP-FET Hello,
I see that there is a customizable hardware project (eZ-FET Emulation IP) for MSP430 devices that support Spy-By-Wire. I believe this particular part number only supports 4-wire…
Part Number: MSP430F2619S-HT Other Parts Discussed in Thread: MSP-FET , hello;
can i use MSP-FET to program the MSP430F2619S-HT 64-pin, and not using the legacy one MSP-FET430UIF.
Part Number: MSP430F2619S-HT Other Parts Discussed in Thread: MSP-TS430PM64 , MSP-FET Hi,
Can I use www.ti.com/.../msp-ts430pm64 and http://www.ti.com/tool/msp-fet to flash/program MSP430F2619S-HT? If not what options do I have?
Regards,
Bezak
For the lead finish, see the "Ordering & quality" table on the MSP430F2619S-HT product page.
For the Au thickness, see [FAQ] What is the thickness of Gold (Au), Palladium (Pd), or Nickel (Ni) for TI's NiPdAu lead finish?
Part Number: MSP430F2619S-HT Other Parts Discussed in Thread: MSP430F2619 , UNIFLASH , MSP-FET Hello,
I have some new MSP430F2619 microcontrollers. So far, each one has had a blank Segment A, which is used for clock timing. As I understand it, the MCUs are…