Part Number: MSP430F4250 Hello,
While experimenting with SD16_A in MSP430F4250, I noticed that the ADC readings for the same input voltage are different when using different clock sources. Why is it so?
Crystal freq= 4MHz, so ACLK = 4 MHz. FLL+ multiplier…
Part Number: MSP430F4250 Hello,
I'm in search of example C codes for MSP430F4250 series uC.
Once I had downloaded a zip file from TI website consisting of the same. It had C as well as assembly code examples for using internal OSC, external RTC osc…
Part Number: MSP430F4250 Hello,
1) MSP430f4250 literature suggests using 32.768kHz crystals with load capacitance 7.0 or 9.0 pF. However, I've a circuit which uses 32.768kHz crystal requiring 12.5pF capacitance (from crystal datasheet). The circuit uses…
Part Number: MSP430F4250 Tool/software: Code Composer Studio Hi,
We need information on how to use DSS of CCS. We are trying DSS as per the Wiki page below. processors.wiki.ti.com/.../CCS_Modules_Library
We would like to know. Q1) How to judge if there is…
Other Parts Discussed in Thread: MSP430F4250 , MSP430-FLASHER Hello,
I have a board controlled by MSP430F4250, which works fine and we need to burn the same code into another MSP430F4250. However, the source code (main.c) got modified erroneously. Since…
Hi James,
Thanks a lot for your reply !!!
ADC channel I set CH_2. when SD16AE = SD16AE2; , I can't read out ADC convert value.
when SD16AE = SD16AE6; , I can read out ADC convert value. You can see I last post picture.
============ code ===========…
Other Parts Discussed in Thread: MSP430F4250 Dear All,
One of our client is using MSP430F4250 with 8 Mhz clock.
They have implemented watchdog reset and are resetting the watchdog periodically about 2-3ms and it is working fine.
But In one of part of the…
Other Parts Discussed in Thread: MSP430F4250 Hello All,
we use a MSP430F4250 for pressure measuring with the SD16_A unit. For some time , we observe that the offset values increase . Even when we make a short between A0+ and A0-, we get ADC values around…
Other Parts Discussed in Thread: MSP430F4250 Hi I use the MSP430f4250
And I take readings from SDA16 channel 0 every 2 Seconds (I use basic Timer)
When the microcontroller take readings works on POWER MODE 0
the rest time the works on POWER MODE 3 (…