Part Number: MSP430F6779A Other Parts Discussed in Thread: MSP430F47187 , MSP430F427 , TIDM-3PHMTR-TAMP-ESD
Refer Application Report "SLAA530–March 2012" figure 17 on page 20 and page19
"2.3.3 ESD Protection Using Series Resistor Consider…
Part Number: MSP430FR6989 Other Parts Discussed in Thread: MSP430F427 , MSP430FR4133 I would like to ask you three questions
1. How can the design of three LC sensors for the MSP430FR6989 of TI achieve anti-magnet interference
2. Compared with MSP430F427…
Other Parts Discussed in Thread: MSP430F427 , MSP430F47127 , MSP-EM-DESIGN-CENTER , MSP430F6736A , EVM430-F6736 Dear All,
I need to design a smart meter. Since I have good experience in designing meter using MSP430F427 & MSP430F47127, so i want to use controller…
Other Parts Discussed in Thread: MSP430F427 Hello,
I am using MSP430F427 , i am putting a pull up on pin no. 44 and 45 (P2.0 and P2.1) with 3.0V battery and 10K ohm resistance. automatically get 1.2V on AVCC and 2.1V on DVCC.
Please help.
Thanks,
Muke…
Hi Stanley,
A good place to start would be to look at communication code examples for the MSP430FR2311.
For SPI communication, it looks like the FR2311 will act as a 4-Wire SPI Master. A code example for that is here .
You can also take a look at code…
Other Parts Discussed in Thread: MSP430F427 Hello all....i am new to msp microcontroller and i m thinking to build a 3 phase energy meter using msp430f427.Can i know how can i read voltage or current using sd16 adc to start.I have tried on my own but could…
Other Parts Discussed in Thread: MSP430F427 , TIDM-TWOPHASEMETER-I2040 , EVM430-I2040S My Controller is MSP430F427 used in energy meter . I am facing problem to calibrate Current , Voltage and Phase Shift. What is the best method of calibration of Voltage…
Hi,
Basically, the MSP430F425 has only 512 bytes RAM, which isn't enough for this project. However, the MSP430F4794 has 2kB RAM, which should be enough to hold the required 0x2DC (732 in decimal) bytes (mentioned in the error message above).
Changing…
Other Parts Discussed in Thread: MSP430F427 Hi,
Currently I am working on MSP430F427 device and I want to know that is there any provision to store some important data in its Flash memory. Let see If I have an integer and I want to store that 2 bytes in…