Hi,
I am using the MSP430F6636 DAC12 to generate 40 KHz ferquency in steps. and facing the problem of distorted wave form( glitches on edges) with DAC amplifier on highest setting(DAC12AMP_7) . while using same hardware circuit and MSP430F4616,there was…
Other Parts Discussed in Thread: MSP430F4616 Hi all,
I am working with msp430f4616 and I would like to know what are the factors that affects the reset vector. Due to some program restrictions I would like it to be fixed, but it is changing after modifying…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave
Other Parts Discussed in Thread: CCSTUDIO I have been trying for the last week to install CCS 5.2 onto a new computer with no luck. It appears some of the features install but not all. I require assistance to the problem. Below is the log.
[ Edited by…