Hello everyone,
I'm writing a program that does SPI transfers to SRAM using DMA. I'm a bit puzzled about the behavior I'm seeing. I set up my processor to run at 16.77216MHz and wanted the SPI clock to run at half that speed (ideally 16MHz…
Other Parts Discussed in Thread: MSP430F47187 We had an earlier board with this processor that would get very accurate reliable results for power measurement capturing multiple analog channels. Ironically, our newer version of the board with "improvements…
Other Parts Discussed in Thread: MSP430F47187 hi,
We have a problem with RTC not working on a MSP430F47187.
Sometimes, (I have found no real raison, but sometimes at PowerUp, sometimes after flashing device and reseting by tool), RTC is not counting. i…
Other Parts Discussed in Thread: MSP430F47187 Hello, everyone.
We faced a problem with MSP430F47187 MCU. USCI_A in UART mode, UCMODEx=00; Baudrate = 9600 (register's values taken from table 19-4 of slau056j.pdf); program is simplest - just one interrupt…
Other Parts Discussed in Thread: MSP430F47187 I am Using IAR Embedded work-bench. I did project for MSP430F47187 in this compiler. My projects code is successfully compiled in IAR. But when I download this code to controller. the controller is not response…
Part Number: MSP430F47167 Other Parts Discussed in Thread: MSP430F47187 Hi champs,
Please advise if customer can replace some tantalum capacitors connecting DVCC, AVCC and LCDCAP pins to VSS.
Application: 3-phase e-meter
P/N: MSP430F47167/MSP430F47187
…
Other Parts Discussed in Thread: MSP430F47187 Dear,
I'm using MSP430F47187. while i am doing program i got map file result as
18 560 bytes of CODE memory 4 951 bytes of DATA memory (+ 126 absolute ) 2 498 bytes of CONST memory Errors: none Warnings…
Other Parts Discussed in Thread: MSP430F427 , MSP430F47187 Hi.
In my task I need to achieve the sampling frequency ~14kHz. In SD-ADC higher OSR providing best filtered results. My colleague built a schematic (on MSP430F427), where he overclocked Fm up…
Hi,
I have a battery in our product which is 3.6V and we have to detect if its voltage is less than 2.5V.
This battery is not going to MSP VDD. So we have to use SVS_IN port of MSP.
Before connecting this battery voltage to SVS_IN we used simple…