Other Parts Discussed in Thread: MSP430F47197 , MSP430F5529 Hi all,
We are working on the project, in which we use SD16A module of msp430f47197 to calculate analog voltage and current.
and after all calculation we want to transmit that values to msp430f5529…
Other Parts Discussed in Thread: MSP430F47197 I trailered the following code to use it for MSP430F47197.
www.ti.com/lit/an/slaa208a/slaa208a.zip
Here is my code:
#include "msp430x471x7.h"
#define SlaveAddress 0x50
#define MAXPAGEWRITE 32…
Other Parts Discussed in Thread: MSP430F47197 , MSPWARE I want to use internal HARDWARE RTC of MSP430F47197, simultaneously with 1 millisecond interrupt on its Basic Timer.
Please suggest link or example code.
Actually I am generating impulse, and calculating…
Other Parts Discussed in Thread: MSP430F47197 I used IAR to compile and debug and also load the firmware into MSP430F47197. Also, recently I've learnt to load the firmware through the JTAG using the MSPFlasher! (without using IAR) And as my MSP has not…
Other Parts Discussed in Thread: MSP430F47197 , MSPWARE There is an uncertainty in here. Do I need to set my PINS to I2C mode according to the datasheet of MSP430F47197 or just set the Clock and Data right for the EEPROM?
CPU + EEPROM
Datasheet
…
I have my RS485 , 6 pin like the following figure depicts.
Also my code is written as follows.
if(UC1IFG&UCA1TXIFG) // If the port is available
{
UCA1TXBUF = '@'; //Send @ character
if (UCA1RXBUF…
Dear Sir,
We have designed one instrument using TI ic MSP430F47197IPZR. But we are not at all satisfied with the controller as instrument doesnt work properly.
We have received many complains from the customers that the instrument is not working properly…