Part Number: MSP430F5252 Dear team,
For MSP430F5252, I think that it may feature a ADC functions from the page of datasheet, but I am also confused by the table 6-1 of the datasheet below, so it would be great if you could give a extra answer.
Thank…
Part Number: MSP430FR2355 Other Parts Discussed in Thread: MSP430F5252
Processor does not reset after SET_PC 0xFFFE is issued in BSL script.
The part is programmed with a simple test code (flashing LED on a timer output, P2.0).
The BSL mode is invoked…
Part Number: MSP430F5252 Hello,
In my design, I came across an issue with the Uart configuration : it seems to have different speeds between multiple devices with the same configuration.
On some of my products, I have a better result with uart with the…
Part Number: MSP430F5252 Hello,
I'm having an issue that I can't explain with my product.
I use an MSP430F5252 with TI-RTOS (tirtos_msp43x_2_20_00_06) and when I set the Uart driver as recommended by the datasheet and this :
I sometimes get…
Part Number: MSP430F5252 Hello,
I'm currently trying to figure out what the problem is with my SD interface and I can't understand what is wrong :
I use a micro SD slot and the SDSPI driver (with TI RTOS tirtos_msp43x_2_20_00_06).
I managed…
Part Number: MSP430F5252
Hello E2E,
I am having trouble setting an interrupt on the GPIO Port 6 pin 3 of the MSP430f5252.
My GPIO configuration is :
GPIO_PinConfig gpioPinConfigs[] = {
// ...
GPIOMSP430_P2_1 | GPIO_CFG_INPUT | GPIO_CFG_IN_INT_FALLING…
Part Number: MSP430F5252 Tool/software: Code Composer Studio Hello,
I would like to create a custom bootloader (without TI RTOS) and use it with an application (with TI RTOS).
How can I do this ?
I would like to use the same link file (.cmd) with predefine…
Other Parts Discussed in Thread: MSP430F5252 , MSP430F5229 I would like to know if I can simply replace MSP430F5229 by MSP430F5252? I will need to have more RAM for my project.
Other Parts Discussed in Thread: MSP430F5252 , MSP430F5239 ear Team,
As per data sheet of microcontroller is assumed that it has 4 spi i.e. A0,A1,B0 and B1 but when i go through your site it mentioned 2 spi
Please clarify the it which is correct
Regards…