Other Parts Discussed in Thread: UNIFLASH , MSPDS , ENERGIA , MSP430F5253 I recently upgraded my computer with the above versions of Code Composer Studio and CCS UniFlash. I use UniFlash to load my code and CCS to debug it. With these latest updates, I now…
Other Parts Discussed in Thread: CC3100 , MSP430F5253 , CC3100BOOST I'm looking at running the simplelink driver in a non-interrupt based environment. Specifically, it will run in a bootloader, which does not use any interrupts. It looks to me like I could…
I'm performing the same steps as you, although I think I've narrowed down the issue. I definitely have differential download enabled, and I performed the following steps:
1) Erase the main memory with CCS Uniflash
2) Download the 1st image via…
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…