Part Number: TI-RTOS Tool/software: TI-RTOS Hi,
I did the following updates:
Installed latest Compiler (16.9.2/MSP430F5259) and updated the it in the project properties.
Opened *.cfg in XGconf and then right click and updated both options in the outline…
Part Number: TI-RTOS
Tool/software: TI-RTOS
Hi,
I would like to use f_findfirst() & f_findnext() APIs of FatFS module.
Per the documentation, I modified _USE_FIND macro to 1 in C:\ti\tirtos_msp43x_2_20_00_06\products\tidrivers_msp43x_2_20_00_08\packages…
Other Parts Discussed in Thread: MSP430F5259 Hi,
I'm using TI-RTOS with MSP430F5259.
After recent update I keep getting the following error message:
"#1965 cannot open source file "<project path>/Debug/configPkg/package/cfg/<project>_pe430X.h"…
Other Parts Discussed in Thread: MSP430F5259 Hi,
I have pretty large MSP430F5259 RTSC project.
Until lately it was debugging fine however in the last days I bump into strange phenomena - when launching the debugger (F11) I see that the program loads but…
Other Parts Discussed in Thread: MSP430F5259 , MSP430F5529 Hi,
I'm using HeapBuf_alloc(nHeapBuf, 1, 0, NULL) to allocate a single block (block size = 6 bytes).
It works well 2-3 times and then it return 0x0000 or 0xFFFFF or other unreal value.
ROV…
Other Parts Discussed in Thread: MSP430F5259 Hi,
I would like to program MSP430F5259 that is powered from 3.3V and its I/Os are 1.8V.
Is such scenario being handled gracefully by the FET programmer ? what would be the JTAG lines voltage in this case…
Hello Robert,
This is certainly an odd use case. I'm going to have to check to see if this is fully supported in this way. I do have two questions here about the setup however:
1. This part is normally used for 5V tolerant I/o. With the voltage levels…
Other Parts Discussed in Thread: CC3100 , MSP430F5259 , ENERGIA I was wondering if there is any MQTT and web-socket client for MSP430 using cc3100?
I noticed that Energia provides a library for MQTT client, but it is dedicated to MSP430F5259. But I use a…
Other Parts Discussed in Thread: MSP430F5259 Hi all,
My application I need to use 3 SPI links (A0, A1, A2) in MSP430F5259 based app.
My questions refer to the use of DMA transfers with SPI links:
How do I deal with 3 SPIs requiring 6 DMA channels (3…
Hi,
I'm using 2.12 which I understand is the latest.
The platform is MSP430F5259
My application does the following:
CS_initClockSignal(UCS_FLLREF, UCS_REFOCLK_SELECT, UCS_CLOCK_DIVIDER_1);
UCS_initFLLSettle(MCLK_DESIRED_FREQUENCY_IN_KHZ, MCLK_FLLREF_RATIO…