Hi Travis, Ryan,
Travis, I will try to update CCS and MSPFlasher. I'll keep you posted. Please note that I work with a custom made board.
FYI, here is my JTAG pin-out:
1. TDO
2. Not connect (NC)
3. TDI
4. VCC ( 1.8V )
5. TMS
6. (NC)
7. TCK
8.…
So here is the solution (tested OK), built using George's and Archaeologist's comments.
In linker cmd file : //set stack size: -stack 384 /* SOFTWARE STACK SIZE */ //define RAM start addr per device datasheet #define RAM_START_ADDR 0x1C00 …
Other Parts Discussed in Thread: CC1120 , MSP430F5309 , MSP430G2553 , TPS62125 , TPS62740 , TPS62120 Hi~
I'm designing a low-power RF modem with battery and MSP430.
As the main power is a battery(Li-ion 3.4Vdc), I want to design a small maximum current…
I have used the LSM303D with MSP430F5309 device in I2C mode (I know, not same devices, but shows that it should work for you). I am unable to share code however.
Other Parts Discussed in Thread: MSP430F5309 Dear All,
I am using MSP430F5309. In my application I use pin P5.0 as an input where i attache motion sensor. If i attache motion sensor then it gives me correct P5IN value.
but i float that pin then it gives…
Other Parts Discussed in Thread: MSP430F5309 I am able to use the MSP430Flasher application to program application code to an MSP430F5309 with no problems.
I also have a custom BSL that I am able to program to the same device using CCS 4.2.5.
When I try…
Other Parts Discussed in Thread: MSP430F5309 Hello,
I am currently using the MSP430F5309 with I2C and UART interrupts. As a test of stability, I am sending in a stream of bytes from the PC, while running the code using IAR in debug mode, as well as monitoring…
Other Parts Discussed in Thread: MSP430F5309 Hi All,
I want to write an SPI master code. Using MSP430F5309, I have to transmit and receive data.
I checked the example codes of for MSP430F5309. None of them includes polling method. I want a code which polls…
Other Parts Discussed in Thread: MSP430F5309 Hello,
I am very new to TI MSP430 processors. I have written a small code for MSP430F5309 having 2 ISRs one for timer A0 and other for USCI_A0.
The compiler is identifying USCI ISR but not for timer. It is…
Other Parts Discussed in Thread: MSP430F5309 Dear All, I am using MSP430F5309 controller with CCS v5 and IAR MSP430(evaluation version). I have some floating point multiplications and divisions in my code. Just 2 or 3 lines of float arithmetic is consuming…