Part Number: MSP430F5326
Hello,
MSP430F5326 acting as a master, I need to have the r/w bit set to Read while transmitting the address as showed herebelow:
But I only succeeded to have r/w bit at 0.
Here is the code:
UCB0CTL1 |= UCSWRST; …
Part Number: MSP430F5326 Hi
Please Help solve the problem. Thanks a lot.
1. The hardware connection is: battery power supply (3.3v) - > button switch (0.5 internal resistance) - > MSP430F5326.
2. The following figure is the voltage change of OBU…
Part Number: MSP430F5326 Other Parts Discussed in Thread: MSP-GANG Hi Ti guys,
In F5xx and F6xx serial, a customer-BSL is supported. I want to know if I erase the TI-BSL, but fail to download a new BSL code , is it still possible to connect the MSP again…
Part Number: MSP430F5326
Hello,
I am using the MSP430F5326 and I would like to do as figure 36.3 of the datasheet:
Send the 7 bits adr + Write, expect the 9th clock cycle to read the ACK or NACK, have de processing delay and send the next byte according…
Part Number: MSP430F5326
The ADC Channel 5(pin 6.5) is always connected to the GND,ADC mode is Single-channel single-conversion,Gathering many times it will occur a nonzero,the code showing as following.Please help to confirm. thanks
#include "msp430f5326…
Part Number: MSP430F5326 Hi all
I am using MSP430F5326 in my new project
I am using it to interface with a sensor with 3 wire SPI connection
Pls help me to connect the MSP to the sensor, using SPI pins of MCU
I have found this for the PIC controller,…
Part Number: MSP430F5326 This should be a simple question:
I am using the Timer_A module to generate a Count Up timer and comparing to the TA0CCR1 register. Here is the code:
TA0CTL = TASSEL1 + ID0 + MC0 + TAIE; // SMCLK/2 Up Mode
TA0CCTL1 = CCIE;…
Part Number: MSP430F5326 Hello,
I am using the MSP430's CRC16 module to generate a CRC value for 24 bytes of data. I would like to compare that data to a Verilog circuit that uses the same CRC algorithm. In trying to design the Verilog circuit, I cannot…
Other Parts Discussed in Thread: MSP430F5326 hi.
MSP430F5326
i need function that the msp will only work from 2.4v and above.
if v=2.39 or less it will not function.
thanks.
Other Parts Discussed in Thread: MSP430F5326 I use JTAG way to program msp430f5326 with reference to slau320 . I use function VerifyPSA_430Xv2 for very fast data block program verification . if the starting address of program verification is 0X8000. verify value…