Other Parts Discussed in Thread: MSP-GANG , MSP430F5341 Hi,
We are using MSP-GANG to program MSP430F5341 devices, We would like to know if it is possible to connect multiple MSP-GANG to a single PC.
Currently we have 3 MSP-GANGs and would like to know if…
Other Parts Discussed in Thread: MSP-GANG , MSP430F5341 Hello all,
I am writing a custom application that uses the MSP-GANG programmer for flashing MSP430F5341 chips, and another batch programmer for flashing other chips on the same target boards. I am able…
Other Parts Discussed in Thread: MSP430F5341 One of my designs uses the msp430f5341 using the Spi by Wire debugging interface and I'm encountering an odd problem I'm having trouble figuring out. My code is toggling a pin from high to low then back to high…
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave