Part Number: MSP430F5342 Other Parts Discussed in Thread: MSP-FET
Part: MSP430F5342
Debugger: MSP-FET
IDE: Version: 7.4.0.00015
We are working on updating an obsolete bluetooth IC which is configured via AT commands (serial commands) from a MSP430F5342…
Part Number: MSP430F5342 Hi Team,
My customer want to activate UART automatically from LPM3 when UART received data.
His using internal REFO as system clock source. ACLK=32.768K, SMCLK=1M. Baud rate is 9600.
But he found that when he use SMCLK as UART…
Hi Yash,
Sorry for late response. As for the BQ device, I suggest you file a new thread in the corresponding threads, I am not the experts of it.
B.R.
Sal
Part Number: MSP430F5342 Other Parts Discussed in Thread: MSP-FET
We have a new product line that was acquired.
It has a MSP430F5342
I am trying to program the microcontroller on the PCBs using the existing JTAG connection points in the PCB in conjunction…
Part Number: MSP430F5342
I'm using MSP430F5342, but there's a problem with JTAG Firmware flash. 1. I put a pull-up resistor 47k in the reset pin, but when I measure the voltage on the pin, I get 0.6V. And Firmware doesn't flash. The same is…
Part Number: MSP430F5342 Other Parts Discussed in Thread: MSPWARE Hi, I am using using a MSP430F5342 micro controller which is connected to 3 temperature sensors via I2C. I believe there should be driver library APIs which will be useful for the development…
Part Number: MSP430F5342
I have an older project.
Was asked to use CCS 7.4.0.00015
When compiled there is warning "Invalid project path: Include path not found (C:\ti\ccsv7\ccs_base\msp430\driverlib\MSP430F5xx_6xx)."
This directory does…
Part Number: MSP430F5342 I'm still have same leakage when sleeping and have new info.
I recently read on a different forum below that setting unused ports as outputs = 0 internal resistor enabled can still allow leakage through moisture or debris picked…
Part Number: MSP430F5342 Hi, I am using MSP430 to read temperatures form the sensors . To convert the digital temperature value read from the sensors to analog using a function which does some floating point calculation. The execution control is not going…
Part Number: MSP430F5342 This is ongoing over multiple board revs and designers over the years. It's showtime for a new product, it's one of the last items, so appreciate any help here. Thanks in advance!
Before getting into the circuits etc, my…