Part Number: MSP430F5342 Dear TI experts,
I am using MSP4305342 and have some strange problems.
I have 50pcs boards,there are two boards run into the unexpected funtion which locates at code segement 0x22400.
This function is doing some "flash erase"…
Part Number: MSP430F5342 Hi MSP team,
I'm posting this on behalf of my customer-
I am looking at a situation where we power the uC at a slow rate. The circuit takes a long time to get from 0V to 3.6V (very slow Slew rate or power on time). For example…
Part Number: MSP430F5342 Tool/software: Code Composer Studio Starting with macOS 10.15 (Catalina), only 64bit executables are supported. But it appears that many of the compilers for OS X, including MSP430 v16.9.11 LTS, which my project depends upon,…
Part Number: MSP430F5342 Other Parts Discussed in Thread: MSPBSL Hello,
I am trying to develop a custom BSL for the MSP430F5342. I downloaded the MSPBSL_CustomBSL430 1_01_00_01 Software package from
http://software-dl.ti.com/msp430/msp430_public_sw/mcu…
Part Number: MSP430F5342 Dear Sir/Madam,
my customer is seeing a +/- 0.1V difference when waiting longer after enabling ADC and settling Vref for MSP430F5342? Anyway to get a stable ADC setup?
The code used to setup ADC:
Initialization:
i. // Initialize…
Part Number: MSP430F5342 Dear TI experts
Now I have some problems when I test the MSP430F5342.
According to the slaz278ab,errata PORT24 says that there will be an increased current consumption because of the internal floating pads.
And Workaround gives…
Part Number: MSP430F5342 Dear TI:
First,
Now I am doing some test on MSP430F5342.
According to the slau208q, I am in doubt about something.
UCSCTL6 Register
It says that "and XT2 is not in bypass mode of operation". If I use the…
Part Number: MSP430F5342 Other Parts Discussed in Thread: MSP-FET Tool/software: Code Composer Studio Hello experts,
I would like to select JTAG mode (2-wire JTAG mode or 4-wire JTAG mode) through CCS 8.2.
I can select JTAG mode through Code Composer Essentials…
Part Number: MSP430F5342 Other Parts Discussed in Thread: MSP430F5529 Tool/software: Code Composer Studio I developed a boot loader that use the SD card for the application update.
I need to compiling and generate a .hex file of the application that start…
Part Number: MSP430F5342 Jace,
I asked the same question on different post then found this post and it 100% matches my question. Sorry for the repeat.
The Custom BSL package contains the released BSL image for the MSP430F53xx famliy. There is no way to…