Hi Mechi,
I2C interface is the necessary way to configurate the blinking function for LP5036 and it need to work continuously. LP5569 is a channels I2C RGB LED driver with engine control and charge pump. It can release the I2C interface after configurate…
We are discussing this issue in the other thread.. https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1341147/msp430f5418a-msp430f5418a/5119641#5119641
I am going to close this…
Part Number: MSP430F5418A Other Parts Discussed in Thread: MSP430F5418 I see that there are differences in the library code.
Can someone list the differences in English?
In the BOM for our product, MSP430f5418 A is listed , but MSP430f5418 is what is actually…
Part Number: MSP430F5418A I have the SPI set up - I send 2 bytes - 0x0F and a dummy byte.
I read the RXBUF and it's constantly returning 0xFF .
Does anyone have code?
I was successful in querying the sensor with the TMS320. Now I have a project with…
Part Number: MSP430F5418A Hi,
ADC12 channels 0-6 are taken for other ADC readings, so I want to output the temperature on ADC12MEM7.
Until now, an external Temperature sensor has been used. I need to read the MSP430's internal temperature sensor. …
Part Number: MSP430F5418A Has anyone experienced this?
I migrated code from IAR (MSP430 Workbench 7.12) to CCS (10.1.1 + MSP430 driverlib 2.91) - and the timers are much slower by a factor of 20.
Is there any known reason for this? Is this at all documented…
Part Number: MSP430F5418A The msp430f5418a specification states that the clock of the system can work normally when the power supply voltage of 12m frequency crystal oscillator is 1.8V; now when 25m crystal oscillator is used, the power supply voltage…
Part Number: MSP430F5418A We are developing the BSL host for MSP430F5418A firmware upgrade from BSL UART. I tested the BSL command but got the response which is different with SLAU319AD :
IC: MSP430F5418A REV F, BSL invocation method: applying BSL Entry…
Yes. The orange color is tricky - but yellow is basically impossible to achieve.
For orange - red-255, Green-40, Blue-0
I also learned that if I use the USCI_B_I2C_masterSendMultiByte... WithTimeout functions - I must check the returned value to determine…