Part Number: MSP430F5437A Hi,
we are using MSP430F5437A for one of project. During initialization we made gpio port 8 as I/O and direction output. Is there any possibility for that port forcefully change that port selection to secondary purpose(TA0 timer…
Part Number: MSP430F5437A Hi,
We are using MSP4305437A where we write a set of logs in the main memory bank 30000-3fff. I am trying to write and erase a set of logs into this location within an ISR routine. Everytime the interrupt comes I write few bytes…
Part Number: MSP430F5437A Hi,
I am working on MSP430F5437A, and observed that while doing an erase and write to Info D memory, a trail of 0's(24bits) is being written into this memory in between that data. This does not happen always and only happens…
Part Number: MSP430F5437A Hello,
I will use this part(MSP430F5437A) for a commercial product.
I found the following information from MSP430 BSL.
If the device is secured by disabling JTAG, it is still possible to use the BSL. Access to the MSP430 MC…
Part Number: MSP430F5437A We are using 3 channels on the ADC. One for a temperature read, one for a battery level, and one for ambient light level. Occasionally we are seeing ADC value that are unexpected. For example a temperature value that works out…
Part Number: MSP430F5437A Other Parts Discussed in Thread: MSP430FR5849 Hello,
I consider redesigning a new product using MSP430F5437A to replace the existing product using MSP430F2254IDA. I need more GPIO pins and ADC channels and would like to reuse HW…
Part Number: MSP430F5437A Hi,
We are doing segment erase in flash and after it is completed by checking busy bit, we are doing Byte-Word write, in data section .infoB.
We repeat the above 6 times and then giving a delay of 4 secs. During this delay of…
Part Number: MSP430F5437A Hi,
I am working on MAP430F5437A for one of my project. When i tried to debug my application with couple break points i am able to see hitting all break points initially but after some time(5-10 min) didn't see code hitting any…
Part Number: MSP430F5437A
Tool/software: Code Composer Studio
Hi, When I launch the debug session of the firmware I want to AUTOMATICALLY add the symbols from the bootloader which resides in same project folder. CCS_Project/ Booloader/bin/bootloader…
Part Number: MSP430F5437A Hello,
I'd like to ask if the following connection of Vcore(MSP430F5437A pin#49) is correct. Please refer to the picture.
VCORE doesn't look like being connected correctly. The datasheet says as follows:
CVCORE :…