Part Number: MSP430F5438A
Hi Team,
I am using MSP430F5438AMPZREP in my design. What is the VIH/VIL for the GPIOs.
I will be using few of MSP430 banks to monitor different power rails. I have Power rails 0.75V, 0.85V and all the voltages higher than 1…
Part Number: MSP430F5438 Can i run the code on code composser studio without having MSP-FET430UIF and directly connecting MSP430F5438 board with my PC? when i do this, it always sAYS
Error initializing emulator: No USB FET was found
Part Number: MSP430F5438 Hello,
I am trying to program MSP430F5438 using BSL programming. Using BSL_Scripter for the same. But it failed to program. Referring MSP430 Flash Devices Bootloader (BSL) SLAU319AE & BSL Scripter document.
In hardware, using…
Part Number: MSP430F5438 Dear team,
The customer want to migrating from MSP430F5438A to MSP430F5438 because of ( MSP430F5438A ) out of stock.
They read the https://www.ti.com/lit/an/slaa419c/slaa419c.pdf and they have several questions.
1 The PMMCOREVx value…
Part Number: MSP430F5438 Hi team,
Here's an issue from the customer may need your help:
Configuration is as follows:
UCA1CTL1 |= UCSWRST; // **Put state machine in reset** UCA1CTL0 = UCMODE_0; // Select the serial port function UCA1CTL0 &= ~UCPEN;…
Part Number: MSP430F5438
Hi team,
Here's some issues from the customer may need your help:
The customer have made a test board, including a F5438, a 32768 crystal with an external XT1, and a regulated chip that consumes 1ua of power. Now the configurations…
Part Number: MSP430F5438 Other Parts Discussed in Thread: UNIFLASH , MSP-FET Hi team,
Here's an issue from the customer may need your help:
UNIFLASH shows for UNKNOWN ACK value when BSL is burned, as shown in the figure below:
The error after swapping…
Part Number: MSP430F5438 Hello,
1) I am trying to program MSP430F5438 using BSL method. As mentioned in SLAU157AS document page no. 61 Allow Read/Write/Erase access to BSL memory, i tried same but in my CCS this option is permanently disabled. How to…
Part Number: MSP430F5438 Team,
My customer has been using the MSP430F5438 and are wondering what exactly will happen if they do not rebuild the code using the 438A version’s header and linker files.
They’re reading the migration guide , but…