Part Number: MSP430F5507 Hello,
A couple questions on the MSP430F5507:
Is there a Boundary Scan Files for this µP?
I have read some literature that the JTAG interface is not 100% IEEE 1149.1 (JTAG) compatible. Is this still true?
Thank you…
Part Number: MSP430F5507 Hello,
I would like to ask Msp430 USB BSL firmware update.
We use the Msp430F5507 on our custom board.
When the OS of PC was "Windows 7", I could do USB BSL firmware update without problems, by using Msp430 Usb Bsl and…
Part Number: MSP430F5507 Other Parts Discussed in Thread: MSPBSL Hello Team,
My customer wanted to confirm if there's any code pre-loaded in the BSL sector? They are aware that you can load your own code in that sector. I f I am understanding this correctly…
Part Number: MSP430F5503 Hello, I have a product that uses the MSP430F5503IRGZR. I would like to use the MSP430F5507IRGZR as any alternate. Is any firmware or hardware change required to use the '5507 version? For example, are any changes required to…
Part Number: MSP430F5507 Other Parts Discussed in Thread: MSP-FET , Hello
I am working on MSP430f5507, currently, I am developing my application using CCS software, MSP-FET for the hardware connection. Now I am reading about the MSP430-BSL and would like…
Part Number: MSP430F5507 Other Parts Discussed in Thread: MSP-FET I am a student at the University of Arkansas and I am trying to use the MSP-FET with Code Composer Studio to program and debug on our target board. Our target board connects to the FET with…
Part Number: MSP430F5507 Hello Team,
Can you confirm the pin1 orientation in the reel of MSP430F5507IRGZR? I looked into the datasheet and I can't find this OPN in PACKAGE MATERIALS INFORMATION page 112. Can you also share the tape pitch?
Regards, Ren…
Part Number: MSP430F5507 My customer is facing the issue of "no communication start of UART at low temp(0℃)" on their system.
The UART communication using the USCI port did not start when the power was turned on occurred,
UART is working correctly…
Part Number: MSP430F5507 Hi ,
I have a code running on MSP430F5507 , everything is working fine. But I have the following concerns:
1- Configure the SPI module UCB1CTL0. While the UCSWRST is 0.
the register is modified without issues.
2- Write/erase…
Part Number: MSP430F5507 Hi, I want to ask about the linker file, I am using the Main flash memory to store some data (3k byte). I am using the segments right below the interrupt vector segment. and the flash region in linker file in within the segments…