Hi all-
I'm just trying to write a "hello world" program that uses printf to output to the UART. Can someone possibly give me some hand-holding instructions to get this working? The tools and versions i'm using are in the subject of the…
Part Number: MSP430F5510 Other Parts Discussed in Thread: MSP430F5515
Hi,
There are some problems for MSP430F5510 related to port state (not high-z) during reset / startup (PORT16 and PORT30) in slaz301s , without workaround. There are present from first…
FYI, I was able to get CCS V5.5 to connect to my MSP430F5515 using the MSP-FET and a special cable that crosses over the pin functions per appropriate diagram at :
Other Parts Discussed in Thread: MSP430F5515MSP430F5515, BSL 06.05.34
I have written a PC-based USB bootloader application that writes a TI.TXT file to my MSP430F5515 custom board. All works correctly except for the last 128 bytes of flash (0x14380 -…
Other Parts Discussed in Thread: MSP430F5515 , TMS320C5515 We have been using the MSP430F5515 in production and have begun to run into serious problems with the USCI in UART mode. The UART bit time errors seem to vary significantly more than they should…
Other Parts Discussed in Thread: MSP430F5515 , FLASHTOOL , MSP430F5510 I am getting ready to release a product to production which uses the MSP430F5515. I would like to secure the code and do understand how to "blow" the JTAG fuse. However, since I will…
Other Parts Discussed in Thread: MSP430F5515MSP430F5515, CCS V5.5
Is it possible to launch a CCS debug session without automatically re-loading code into memory? I would like to debug the code that already exists in internal flash.
Other Parts Discussed in Thread: MSP430F5515 I am trying to debug what appears to be a boot problem with my custom MSP430F5515 board. However, each time I connect to the target the CPU is stopped and reset by CCS, even if I have disabled those options…