Other Parts Discussed in Thread: CC3100MOD , CC3100 , MSP430F5521 In the user guide I see that in order to program the serial flash in the CC3100MOD or if we will use the CC3100, it needs to be done using the UART interface?
or it can be done from the SPI…
Other Parts Discussed in Thread: MSP430F5521 Hi,
I am sorry to ask the same question... With respect to MSP430F5521 I would like to know what could happend to the device if we use 0.1uF instead of 400nF as per the datasheet?
One of our customer has unfortunately…
Other Parts Discussed in Thread: MSP430F5529 , MSP430F5521 Hi,
In the application MSP430F5521 and MSP430F5529 are interacting over the UART.
We do have five systems in lab, all the systems are loaded with the following configuration settings as shown below…
Other Parts Discussed in Thread: MSP430F5521 MCU: MSP430F5521
I am using SPI on USCIB0 to send bytes to an MCP2515 CAN controller. Chip select is pulled low by a function to initialize the SPI transaction. The Tx interrupt loads bytes from a software buffer…
Other Parts Discussed in Thread: MSP430F5521 I've got a serious problem involving the MSP430F5521 and the USB connection. When the supply voltage is 3.3V and plug in and unplug the USB a few times in sequence, the MSP430F5521 is warm (150 degrees Celsius…
Hello Jeff
Thank you,
I tried with the latest version Rev E and it works fine.
However we will be using MSP430F5521 in our final production.
And the above issue is still there in case of MSP430F5521 Rev E .
I have also tried MSP430F5522 Rev…
Hi Lisa,
the Lunchpad is come from TI, no changes are made.
The msp430f149 has a 4W-JTAG and uses the standard implementation of TI. The msp430F5521 uses also 4W-JTAG but supportes SBW too.
That means, if CCSV5.1 only works with SBW, then it can not…
Other Parts Discussed in Thread: MSP430F5521 , MSP430F5437A Hi,
The user guide "SLAU208H" mentions that ADC has "Auto Power Down" feature which
automatically disables core when not actively converting.
But in some MSP430's sample…
Other Parts Discussed in Thread: MSP430F5521MSP430F5521 has internal flash of 32Kb and 8k of SRAM. Presently ur source code size is 16Kb. We have one requirement to store some data into the internal flash periodically say once in a week (some 12 bytes…
Other Parts Discussed in Thread: MSP430F5521 Hi!
I ‘ve been working with the MSP430 USB DEV PACKAGE using HID DATAPIPE interface.
I am using MSP430F5521.
I am having an reception issue (device side) when the data packet is bigger than the…