Part Number: MSP430F5524 Hi TI experts,
Application : E-Cigar
status : MP
This project was mass-produced 1M in 2018. This year, they started production again at the request of end-buyers.
Their production plants measure the standby current of the board…
Part Number: MSP430F5524 I have created a prototype board and application. All issues have been resolved except for this: I need to run the BSL as an integral part of POR to detect corrupted software during software upgrades. According to slaa457b.pdf…
Hi David,
Thanks for going through the code. This was the existing code when I joined my workplace and because it was working, I let it be. I had been thinking of changing it as well. While it can be improved, there is no obvious error with it that should…
Part Number: MSP430F5524 Other Parts Discussed in Thread: MSP-FET My project is complete with a functioning BSL and USB. However, I have some issues with power-up that are recoverable, but I would rather that my customers never see. To determine if these…
Part Number: MSP430F5524 Other Parts Discussed in Thread: LDC1612 Hello
My customer is communicating with LDC1612 using I2C of USCI_B1.
During the I2C communication, there was a problem that the start bit did not occur, and as a result, it was confirmed…
Hi Abhishek,
just to avoid misunderstandings on this point, the two while loops
// Wait till SVM is settled while ((PMMIFG & SVSMLDLYIFG) == 0); ...... // Wait till new level reached if ((PMMIFG & SVMLIFG)) while ((PMMIFG & SVMLVLRIFG) == 0);…
Part Number: MSP430F5524 I am having certain "defective" ICs with me which are unable to handle a clock speed of 16MHz. The code stops running after a while and I am unable to pause the program in the debugger giving me the error message
I thus…
Part Number: MSP430F5524 Pins 3.3, 3.4, which were being used for UART, have suddenly stopped working. Using them as GPIO pins is also not working. The remaining pins, functionalities appear to be working fine.
I had observed the UART not working with…
Part Number: MSP430F5524 Hi
I am generating a PWM to turn on a fan. Here is the code
TA2CCR0 = 1000; // PWM Period TA2CCTL1 = OUTMOD_7; // CCR1 reset/set TA2CCR1 = 900; //384; // CCR1 PWM duty cycle TA2CCTL2 = OUTMOD_7; // CCR2 reset/set TA2CCR2 = 900;…
Part Number: MSP430F5524 (I am reposting this because the first time I posted it selecting that the problem was in CCS. I am not sure if that is the case and if the former post would be visible to the public at large.)
I am facing a pretty weird situation…