Other Parts Discussed in Thread: MSP430F5528 , MSP430F5524 Hi,
I'm using MSP430F5524 to communicate with MSP430F5528 via UART. How can i do a field firmware update on MSP430F5528 with MSP430F5524? The only USB connection is connected to MSP430F5524 and…
Other Parts Discussed in Thread: MSP430F5524 I am using the MSP430F5524 and have custom code that was developed by a third-part developer. I am in limited production and have built 50+ boards successfully. But I have a problem with one board that always…
Hi David,
did you manage to solve your issue with the PU port? I am running exactly into the same trouble!
I want to use the pins PU.0 and PU.1 as GPIO (I am using MSP430F5522).
I want to give the 3.3V externally to the VUSB pin, leaving the VBUS unconnected…
Other Parts Discussed in Thread: MSP430F5524 We are having a problem with MSP430F5524 and
Question 1
========
In a normal behaviour, RST signal of a microcontroller with a 3V3 power supply is expected to be at 3V3.
We had a board running correctly for…
Part Number: MSP430F5528 Other Parts Discussed in Thread: MSP430F5510 , MSP430F5524 , MSP430F5526
I just need some confirmation. Is my understanding that the following devices are P2P equivalent, both from a hardware and software point of view? The difference…
Other Parts Discussed in Thread: MSP430F5524 , MSP430USBDEVPACK Does anyone know of or have firmware that will make the MSP430f5524 into a USB to Serial Chip? Or any suggestions as how to go about writing some?
I need to be able to update the firmware…
Customer is evaluating technical specifics of the 5524 as a replacement for the 5324, since the 5324 may not be available when they launch.
One technical difference that may be an issue is the bootstrap loader (BSL). The 5524 supports either USB or UART…
Other Parts Discussed in Thread: MSP430F5524 , MSP430F148 I have an old design that used the MSP430F148. Its board includes a high density connector that includes the JTAG pins and is used for programming the device during manufacturing. I am making a new…
Other Parts Discussed in Thread: MSP430F5524 I am using MSP430F5524 in our products and it is in production stage. Each USB port of these MSP430F5524 parts needs to be tested. Most of computers I used to test this function have no problem. However, there…
All,
I have noticed the non-linearity
issue that is discussed in errata ADC27 ( SLAZ054C–July
2009–Revised July 2010 ).
The fix for this is to output
the internal reference voltage. I have demonstrated that this fixes my
non-linearity…