Other Parts Discussed in Thread: MSP430F5526 I have successfully created a custom bsl and an application for the msp430f5526. Both work just fine as stand alone applications. However, when I try to combine the two ti text files as a single code file, something…
Other Parts Discussed in Thread: MSP430F5510 , MSP430F5526 I'm having some difficulty calculating the correct checksum values for the BSL. I'm currently using the msp430f5526 (but will also be using the msp430f5510). The formula given in slau319…
Hi,
Regarding the Workaround of CPU26 errata in MSP430F5526.
The Errata sheet mentions, "Write the op code for a NOP as the first instruction on the stack. Begin the intended subroutine at address SP + 2"
In order to do the Workaround should we…
Other Parts Discussed in Thread: MSP430F5526 Hi
I'm using a MSP430F5526 and I've got a Digital IO connected to P5.1/A9/VeREF-. I don't use the VeREF- as the negative reference, all my AD conversions are done with SREF set to 0 (using AVCC and…
Other Parts Discussed in Thread: MSP430F5526 i'm working MSP430F5526, i recently shifted to CCS4.1 from CCE. i want to know whether simulator is present current version. If so, can anyone guide me how to make use of it.
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
Hi Louis,
the lastest SW-version for MSP430-GANG ( http://focus.ti.com/docs/toolsw/folders/print/msp-gang430.html ) is V1.51!
This version has support for new devices: MSP430F5513, MSP430F5514, MSP430F5515, MSP430F5517, MSP430F5519, MSP430F5521, MSP430F5522…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…