Part Number: MSP430F5638 Using CCS v10.4 and msp430f5638 on a custom SBC. I've created two ADC12 read functions, which are derived from two TI examples.
run_430_ADC_T() which is derived from msp430f55xx_adc_10.c and reads a single channel for the internal…
Part Number: MSP430F5638 Using CCS v10, and currently have an MSP430F5638 running on a custom SBC. Using TB0 to create PWM for LED dimming. TB0 is working fine, getting the desired frequency and duty cycle on scope. But I have a number of questions. I…
Part Number: MSP430F5638 Other Parts Discussed in Thread: MSP-FET Using CCS v10, MSP-FET and the MSP430F5638 running on a custom SBC. After the program runs, occasionally the boot.c file will open and the exit() function will be highlighted even though…
Part Number: MSP430F5638 Other Parts Discussed in Thread: MSP-FET Using CCS v10 and an MSP430F5638 running on a custom SBC driving an LCD. Code, board, and LCD were running fine. Using MSP-FET to program the MCU.
Normal use:
Build code ok, Run Debug and…
Part Number: MSP430F5638 Other Parts Discussed in Thread: MSP430F6638 I've designed and built a custom SBC using 1 msp430f5638 which is driving a 480x272 graphical LCD. All is working pretty well, but the LCD redraws the entire screen slowly. By default…
Part Number: MSP430F5638 Hello everyone, I'm using a custom board with a MSP430F5638 an USB BSL for flashing.
The MSP430 USB Firmware Upgrade Example GUI application works fine with this board it flashes successfully and as a result my project works…
Part Number: MSP430F5638 The problem is I can't run USB BSL on my custom PCB board with the MSP430F5638 device. Since the USB BSL needs XT2 oscillator, I've checked signals on pins XT2IN, XT2OUT where crystal oscillator 8MHz is connected, but just…
Part Number: MSP430F5638 Tool/software: Code Composer Studio I’ve designed six Allegro A3214LUA-T magnetic proximity switches into a custom single board computer. Currently have two identical PCBs running. I’m using these switches to generate interrupts…
Part Number: MSP432E401Y Other Parts Discussed in Thread: MSP430F5638 , CC3235S What is the maximum solder and desolder temperature for these MCU's?
MSP432E401Y in PQFP
MSP430F5638 in PQFP
CC3235S in PQFP
And how far above these max recommended temperatures…
Part Number: MSP430F5638 Tool/software: Code Composer Studio Dear team,
1 The customer uses a 1.54-inch color screen, a resolution of 240×240 and an 8-bit parallel port. He found that the refresh rate is very slow.
What solutions are there?
2 The…