As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Part Number: MSP430F6747A
Hi everybody,
I would like to use http://www.ti.com/tool/download/MSP430-ENERGY-MEASUREMENT
now about if this toolkit:
Can perform for higher frequencies, such as 5kHz, which is similar to 50/60Hz?
Does it supports an AC signal…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave