Part Number: MSP430F67641 Other Parts Discussed in Thread: TIDA-01088 , EVM430-F6779 Dears
We need a power calculation chip for the meter to detect the power consumption of the 220V AC input port. I found the TIDA-01088 solution, please help to determine…
Part Number: MSP430F67641 Hi,
I am looking for a document that shows the maximum recommended re-flow profile temperature for MSP430F67641.
Best Regards
Hi Lucy,
The documents that Gary shared with you are the best resources for your questions. The commands may differ slightly since this is a design based on a different device, but they should be similar.
Honestly, the best way to understand how the protocol…
Hello Superpanky,
Thanks for your post. First, I would sniff the UART communication (with the EVM430-F67641 disconnected from the high voltage AC obviously) at the TX_EN and RX_EN headers located between the RS-232 and isolation circuitry and the MCU…
Part Number: MSP430F67641 Hello,
I don't see the switching characteristics information of SD24_B on datasheet, such as data setup time, hold time..etc, we need this information to select proper external modulator when using bit stream interface.
…
Part Number: MSP430F67641 Other Parts Discussed in Thread: MSP-EXP430G2ET , MSP-ISO , EVM430-F67641 Hi, I established connection between energometer EVM-F67641 and my launcphad MSP-EXP430G2ET through UART/RS-232. By using Serial port utility I can see HEX data…
Part Number: MSP430F67641 Dear team,
We have used the MSP430F67641IPN as a 3-phase 4-wire application(see below picture), but we are looking for a solution or refer design for a 3-phase 3-wire application (see below picture),whether have you this solution…
Part Number: MSP430F67641 Other Parts Discussed in Thread: EVM430-F67641 , MSP430F449 , Hello:
I have a question and need some help about the chip of msp430f67641, The meter specification is 10(100)A, const is 500 k
When the meter power on with large…
Also, be careful which UART ISR you're trying to debug (there are several that depend on the type of module). Here, the MSP430F67641 has EUSCI_A2, so this module's ISR code starts on Line 664.
Regards,
James
MSP Customer Applications
Part Number: MSP430F67641 Tool/software: WEBENCH® Design Tools Hi,
For the source code of three-Phase Energy Measurement system (slaa621c), whether can provide its use notes and some Flow chart? so that I can use these code to my application.
I think…