Part Number: MSP430F6779A Because our device needs approximately 600 ms to wait for a stable 32768 Hz crystal.
What happens when using the RTC_C module during the crystals is unstable?
Will fail-safe operation of the UCS module switch the RTC module…
Hi Vasu,
The recommended voltage around the MCU should only be 3.6V, if you're seeing larger than that there may be multiple power sources causing this. Below are the maximum ratings, if you exceed these values the device can be damaged.
I would…
Hi,
Really sorry for the late response. I somehow missed this message.
You can use AUXOK register to instead of AUXSW register to indicate the DVCC status. It should not occur any other issue when using AUXOK register. I do not find related information…
Part Number: MSP430F6779A I have some question about Compiler Resolved defects in MSP430_20.2.5.LTS*.
software-dl.ti.com/.../README.html CODEGEN-7956 Compiler incorrectly elides short-circuit behavior of && when right operand might invoke undefined be…
Part Number: MSP430F6779A as we have use ccs IDE with low level process initial function _system_pre_init that stop watchdog below.
#1 Stop watchdog in _system_pre_init
int system_pre_init(void)
{
/* Insert your low-level initializations here *…
Part Number: MSP430F6779A as we have setting the reset pin to NMI for prevent PMM26
int _system_pre_init(void)
{
/* Insert your low-level initializations here */
__disable_interrupt();
WDTCTL = WDTPW+WDTHOLD;
// Clear RTCHOLD Bit after reset
RTCCTL0_H…
Part Number: MSP430F6779A Is there specification about VLO Clock start-up time?
After reset, How long do we have to wait for the VLO clock to stabilize?
Part Number: MSP430F6779A
What happens if the WDTIE bit and GIE bit are set while WDTTMSEL is 0 (Watchdog mode)?
Can watchdog interrupts occur in watchdog mode?