I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Part Number: MSP430FR2476 Other Parts Discussed in Thread: MSP430FR2676 Hi experts,
Which one is the correct capacitance value for 32kHz crystal oscillator?
Regarding the attached document, CL1 and CL2 are 23pF based on the calculations. On the other…
Hi Cherry,
Attach some document as your reference:
0451.MSP430™ 32-kHz Crystal Oscillators.pdf
MSP430™ LFXT1 Oscillator Accuracy.pdf
Thanks!
Best Regards
Johnson
Hi Paul,
I use the MSP430 product selection page from https://www.ti.com/microcontrollers-mcus-processors/msp430-microcontrollers/products.html and save all parts in the spreadsheet. I use the filters to filter out parts. There are quite a few that…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use the…
Hello Pavel,
EDIT: I didn't read past your first error. You already did this, and I didn't notice.
Pavel Hristov said:
We tried adding the following lines in io.h
#elif defined(__ MSP430F6726 __) #define __MSP430_6726__
For your first error…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );
Which…
Other Parts Discussed in Thread: CCSTUDIO I have been trying for the last week to install CCS 5.2 onto a new computer with no luck. It appears some of the features install but not all. I require assistance to the problem. Below is the log.
[ Edited…