Part Number: MSP430FG439 Hi team,
Is it acceptable in below cases? Because there is a possiblity LCD's SEG pin and COM pin might become shorted in customer's use case.
1. S0 and S1 are shorted.
2. S31 and COM0 are shorted.
3. COM2 and COM3 are…
Part Number: MSP430FG439 Hi
The latest revision of the MSP430FG439 device is E.
Will my customers always receive a revision E device if they purchase this device from now on?
They don't want to use revision B because revision B of MSP430FG439 has a deadly…
Part Number: MSP430FG439 Hi..
We made custom board with MSP430FG439 and INI321 and connect to PC serial port.
I think that MSP430 send ADC data very quickly.
So, PC application lost some ADC Data.
Is it possible flow control between MSP430 and PC uart…
Part Number: MSP430FG439 Other Parts Discussed in Thread: ADS1292 , AFE4960 Hello TI experts,
my customer is looking for the IC that can measure ECG and heart rate using electrode.
there are several ICs that can measure ECG using electrode, but I cannot…
Part Number: MSP430FG439 Hi,
Good Day. I have a customer who is working with MSP430FG439. Please see below his query for your reference. Thank you very much.
I have only evaluation license for IAR EW - MSP430 v7.21 to download the software....but unfortunately…
Part Number: MSP430FG439 Tool/software: Code Composer Studio Dear team,
My customer want to measure the frequency of ext signal with timer capture mode.
Hardware: MSP-FET430U80 with FG439
XT1=32.768kHz XT2=4MHz
Code:
#include <msp430fg439.h>
#include …
Part Number: MSP430FG439 Other Parts Discussed in Thread: MSP430FG437 Tool/software: TI C/C++ Compiler
Hi,
I am now working with MSP430FG439. The data I obtained from LABVIEW_GUI(SLAA458) is pretty good. However, the SLAA458 does not allow me to…
Part Number: MSP430FG439 Tool/software: Code Composer Studio Hi,
I am now working with MSP430FG439 by the pulse oximeter made by myself. The pulse signal I obtained through Labview_GUI(slaa458) is pretty good. In order to further analysis the data, I…
Part Number: MSP430FG439 Other Parts Discussed in Thread: MSPWARE , Tool/software: Code Composer Studio Hello,
I'm trying to use a MSP430FG439 and would like to know if it is possible to use the MSPWare Driverlib but this device is not supported.
Can…
Part Number: MSP430FG439 Other Parts Discussed in Thread: MSP430G2553 , CCSTUDIO Hi,
I need to connect a 2.8" TFT 240 X 320 v1,1 (TJCTM24028-SPI) LCD display via SPI to MSP430FG439. I'd like to know how to do this.
I appreciate any reply.
Thanking…