Other Parts Discussed in Thread: MSP430FG4616 IAR 5.40.1
MSP430fg4616
I am able to debug without downloading, but not download and debug.
This is an old assembly I'm trying to modify so it obviously had debug firmware loaded.
This is very weird.
Any…
Other Parts Discussed in Thread: MSP430FG4616 , MSP430FG4618 Hi,
I would like to ask, has msp430fg4616 ADC12CTL2 register? How can I represent results as 2s complement?
Regards,
Admir
Hi Ernesto,
From what I can see, you need p2p and the same features with extra RAM?? Am I correct. Unfortunately we do not have drop in available for the that device.
If you only need p2p + more RAM, you may want to take a look at the msp430fg4616 , m…
Other Parts Discussed in Thread: MSP430FG4616
I am ajit sonawane .i am trying to download program in MSP430FG4616 its gives the following error also Hex file of program not generate i also check all setting about Hex file all setting correct.
please help…
You are right the address they wrote with extra zero, there was a typo ,please read it as 0x100e8.
Please guide which exe should I use to update the code through BSL mode. Please send me that exe file if possible.
They are using MSP430F2616, MSP430FG4616…
Other Parts Discussed in Thread: MSP430FG4616 I ajit want to generate 125nano timer interrupt in CCSV5 using C language
plz suggest me how to generate nano timer interrupt timer
Used MSP430FG4616
#define Tmr_A_Cnt 1
timer inti.
TACTL = TASSEL_2 + MC_1…
Other Parts Discussed in Thread: MSP430FG4616 , MSP430F2616 , MSP430F4794 , MSP430FE4272 , MSP430F447 Dear Sir/Madam, Currently we are using various MSP430 devices in our products, which are namely - MSP430FG4616, MSP430F447, MSP430F2616, MSP430F4794, MSP430FE4272…
Other Parts Discussed in Thread: MSP430FG4616 , MSP430FG4617 , MSP430FG4618 , MSP430BT5190 in the page of MSP-EXP430F5438 it said
"It features a 100-pin socket which supports the MSP430F5438 ( datasheet ) and other devices with similar pinout."
does…
Other Parts Discussed in Thread: MSP430FG4616 Hello,
I am currently having an issue with getting my ADC started up on the MSP430FG4616. I have tried intializing the port as well as the AD Converter but the values being read in do not correspond to what…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…