Part Number: MSP430FG6426 Hi Team,
We have a usecase where we need to retain few bytes of data in the backup ram memory even during power down.
I have used a 3V battery in VBAT terminal (VBAK not used-Open) and XT1 32Khz crystal not mounted which mean…
Part Number: MSP430FG6426 Dear Team,
We see different conflicting information for this controller " MSP430FG6426IPZR " on the maximum operating frequency.
The product homepage shows 25Mhz https://www.ti.com/product/MSP430FG6426/part-details/M…
Part Number: MSP430FG6426 Dear Team,
I have a function (Function_1) that inturn calls another function (Function_2) and while the final leaf function is executed and return back to the caller function, the local function parameters are not restored. Manwhile…
Part Number: MSP430FG6426 Dear Team,
I have MSP430FG6426 actuating around 80 inductive loads (each 25mA) activated through a comination of TI's 74HC595 shift register and ULN2803.
I get the debug session running very fine while activating the ULN channels…
Part Number: MSP430FG6426
Question №1. How to understand parameter, recovery time "tend", in the document "slau208q MSP430x5xx and MSP430x6xx FamilyUser'sGuide", it is specified in chapter "7.3.2.7 Block Write", on page 355, paragraph 2. In SLAS874B page…
Part Number: MSP430FG6426 Hi all,
I am trying to build and use an RTOS driverlib for the MSP430FG6426 processor which is not built for out of the box.
I keep seeing this link posted around in many responses from TI support and others but the link is now…
Part Number: MSP430FG6426 I wish to acquire single-ended signals in ratiometric mode.
I see CTSD16 works with internal VREFBG (1.16V) or external VEREF+ (1,25V). The internal VREFBG can be used externally from pin VREFBG (REFON = REFOUT = 1) with max 1…
Part Number: MSP430FG6426
Hello!
Help to understand a problem. Transfer of the data from ADC by means of DMA does not work at bit setting "Gie". In the resulted text of the program and a global interrupt disabling//"__bis_SR_register(GIE+LPM0_bits…
Part Number: MSP430FG6426 Hi,
Am trying to use ADC of MSP430FG6426 i.e CTSD16. I am getting some reading in CTSD16MEM0. However it is not the decimal value corresponding to the input voltage. Here I have used internal reference voltage i.e 1.16V. so I…
Part Number: MSP430FG6426 Other Parts Discussed in Thread: MSP430G2553 , , MSP430WARE Hello, I would like to implement "SMBUS" on our desired MSP430FG6426 micrcontroller. But so far, I get a sample code of SMBUS for MSP430G2553. I try to do the porting of…