Part Number: MSP430FG6626 Hi Team,
Good day. I am posting this inquiry on behalf of our customer.
"I am using a MSP430FG6626IPZ. I would like to put out a constant clock at or close to my system clock, around 20MHz. Which IO should I use? Should I use…
Part Number: MSP430FG6626 Hi,
Good Day. May I know if it is possible to build the Ethernet Bootloader for MSP430FG6626?
Please advise. Thank you very much.
Best Regards,
Ray Vincent
Part Number: MSP430FG6626 We currently have an MSP430FG6626 in our design and we ended up connecting an external 3V reference to the P5.0_VREFBG_VeREF+ pin. Upon further reading in the datasheet, although not totally clear to me, it would appear that…
Part Number: MSP430FG6626
We are looking for some feedback on achieving the currents specified for LPM3.
We have a long established product, and are developing a new product based on it. Battery life improvement is a major goal.
After stripping down…
Part Number: MSP430FG6626 Other Parts Discussed in Thread: UNIFLASH , MSP-FET Hi,
I'm using MSP430FG6626 MCU.
Attached schematics which I have captured from the reference document SLAU278AH.
For detailing the schematics I used page 169 of document SLAU278AH…
Part Number: MSP430FG6626 Other Parts Discussed in Thread: MSP430FR2633 Hi,
Is the MSP430FG6626 powerful enough to compute FFT after the signal is captured with the delta-sigma ADC?
Any specific resources/library required for this?
Thank you,
Geoffrey
Part Number: MSP430FG6626 Selected MSP430FG6626IPZ for my keypad project.
1. I would like to drive an optocoupler by the port pin of the MCU, how much current the MCU can sink to drive the optocoupler LED.
2. How much capacitor value should be there on…
Part Number: MSP430FG6626 Hi,
If GSWx bit is set to 1, Is shared GPIO pins unavailable?
For example, When the GSW0 is set to 1, can I use the P7.6/CB10/AD3+/G1SW0 port as P7.6
According to user's guide, if ground switch output is shared with a digital…
Part Number: MSP430FG6626 Hi,
I have two questions about the MSP430FG6626.
1. UART & LCD
the MSP430FG6626 support 2ch UART, but these are shared with LCD port.
(Yellow is uart port, green is lcd port)
P8.3/ UCA1RXD /UCA1SOMI/ S12
P8.2/ UCA1TXD /UCA1SIMO…