Part Number: MSP430FR2155 Hi Champ,
I am asking for my customer.
How are the CHK and CHL in BSL Command calculated ?
I search for the information in below screenshot and want to make sure is TI BSL is calculated using the CRC-CCITT algorithm, correct …
Part Number: MSP430FR2155 Can I burn a program through a string when burning a program for the first time? The external terminal data of the equipment designed by our customers is limited. We plan to burn the program through the serial port during the…
Part Number: MSP430FR2155 Hello,
I'm using a MSP430FR2155 to implement some basic I2C read/write functionality for my application. The MSP430 is configured to be a slave device. My setup consists of an Aardvark I2C device, configured as a master to read…
Part Number: MSP430FR2155 Other Parts Discussed in Thread: MSP430FR2355 , Working on a project that uses an MSP430FR2155. With the current shortages, we would like to add the MSP430FR2355 for alternate builds. This device is the same as the 2155 except for…
Part Number: MSP430FR2155 Other Parts Discussed in Thread: MSP430FR2355 , Hello Guys,
Good day.
Our customer needs MSP430FR2155TDBTR. They are considering replacing the part with an MSP430FR2355TDBTR.
If they compile a .bin file in Code Composer with the project…
Part Number: MSP430FR2155 Hi ,
I am trying to use MSP FET Flash Emulator tool to program the MSP430FR2155TRHAR controller on my PCB.
As I don't have much knowledge on the firmware setup, could you please let me know if I need to install any drivers to…
Part Number: MSP430FR2155 Dear Team,
I just have a short question regarding the internal ADC reference voltage usage.
I have a usecase where i will be performing ADC conversions every 10ms once on all ADC channels. But the point is that i will have to…
Part Number: MSP430FR2155 Other Parts Discussed in Thread: MSP430G2553 , Hello,
I am trying to implement SPI communication using MSP430FR2155 microcontroller by setting the SPI frequency to 8MHz. But I am not able implement it. I have found some SPI code…
Part Number: TIDA-010208 Other Parts Discussed in Thread: MSP430FR2155 Dear Sir/Ms.
Can you give me the source code of MSP430FR2155 in TIDA-010208? I provide TIDA-010208 reference design to my customer RD, and the customer me for the source code.
Best Regards…
Part Number: MSP430FR2155 Other Parts Discussed in Thread: MSP-FET , MSP-EXP430FR2355 , MSP430FR2355
Hii,
i was using MSP430FR2155 Controller,when i was trying the flash the code below mentioned two errors are coming,
1.Error Initializing Emulator : Interface…