Part Number: MSP430FR2475 Hi,
I want to confirm that if I disable the BSL by writing 0x55555555 to address 0xFF84 in FRAM for the MSP430FR2475, will mean that it is unable to be accessed by I2C or UART. I haven't filled up the BSL configuration register…
Part Number: MSP430FR2676 Other Parts Discussed in Thread: MSP430FR2475 Hi team,
There is one industrial project which uses MCU msp430-FR-2475TPT having 32KB of FRAM and 6KB of RAM. Now the firmware is implemented completely for msp43-FR-2475TPT, but…
Part Number: MSP430FR2475 Other Parts Discussed in Thread: UNIFLASH , MSP-FET
I have a MSP430FR2475 device where by writing 0x55555555 to JTAG signature 1 and 2 (i.e. to address 0xFF80) I have been able to lock down JTAG access. I have also written 0x55555555…
Part Number: MSP430FR2475 Other Parts Discussed in Thread: MSP-FET Hi TI team,
I would like to request help using the backchannel UART of the MSP-FET debugger connected to the MSP430 microcontroller, please refer to our schematic below for the discussion…
Hi! I have an MSP430 project for which I wanted to maintain two sets of builds (e.g. a 'developer' and a 'customer' build) based on different preprocessor directives. We are using Code composer studio to generate our builds. I created a new build configuration…
Part Number: MSP430FR2475 Hello,
I have a few questions about the I2C driver code in the resource explorer for MSP430FRxxx.
1. In the MSP430 example code for the I2C driver, I found a function called 'CopyArray'
```
void CopyArray (uint8_t * so…
Samyukta Ramnath1 said: Hi Brandon Fisher94 , the piece that I'm not understanding or the piece I would like to confirm, is that Uniflash is sending this JTAG User_Code_Erase command that must be applied through the JTAG mailbox. Could you point me to…
Part Number: MSP430FR2475
Hi team,
Currently we are using a 4.7K pull up on the I2C lines of the MSP. We have 2 I2C lines/MCU and both operate at 400KHz frequency.
When we were doing the validation, we found that the rise time is more than the general…
Part Number: MSP430FR2475 I don't know why I can't clear XT1OFFG.
I wrote the following code based on the link below, but I can't get out of the while and clear the flag. What is the possible problem?
MSP430FR2433: XT1 Clock Operation and…