Part Number: LP-MSP430FR2476 #include "driverlib.h"
void main (void)
{
//Stop watchdog timer
WDT_A_hold(WDT_A_BASE);
//Set LED1 to output direction
GPIO_setAsOutputPin(GPIO_PORT_P5,GPIO_PIN0);
GPIO_setOutputHighOnPin(GPIO_PORT_P5…
Part Number: MSP430FR2476 ACLK ~32kHz, DCO=MCLK = SMCLK = 4MHz What would the code look like if I wanted to configure it as above? There were some parts in the sample code that were difficult to understand. I would appreciate it if you could provide me with…
Part Number: LP-MSP430FR2476 Other Parts Discussed in Thread: MSP-FET , MSP430FR2476 I would like to monitor the ACLK, SMCLK, and MCLK clocks using the sample code "cs_ex1_DCO1MHzSWTrim". No clock waveform is output to the corresponding pins "P2…
Part Number: LP-MSP430FR2476 When using P2.3 of LP-MSP430FR2476 as an input pin GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P2,GPIO_PIN3); If I enable the internal pull-up resistor, it will work without any problems, but Since there is an external pull…
Hi Kenley
The pins are grouped into upper and lower segments, so selecting “lower” or “upper” will filter the available pins based on that selection. We are checking if there is any document to explain where it specifies if a pin…
Part Number: MSP430FR2476 Other Parts Discussed in Thread: MSPBSL , MSP430FR2311 , Hi Team,
I am working on BSL code and able to flash the code correctly on the same location of the memory(0x8004).But I have two applications and both the applications uses…
Part Number: LP-MSP430FR2476 Hi Team,
I am working on BSL code and able to flash the code correctly on the same location of the memory(0x8004).But I have two applications and both the applications uses WDT so when running two applications it is problem…
Part Number: LP-MSP430FR2476 Using the sample program "timer_a_ex6_upDownModeOperation" as a reference, how should I change the code if I want to use upDownMode and blink the LED at 2 second intervals? In particular, how do you enable interrupts…
Part Number: MSP430FR2476 hi team,
Previously we are using MSP430FR2476TPT part number as an microcontroller in our project, Now we need to find alternative to this part which Safety integrity level (SIL) certified microcontroller. kindly suggest alternate…